The Keysight CX3300 series Device Current Waveform Analyzer now offers two new sensors that enable the characterization and validation of power delivery network (PDN) devices up to 100A. This extended range allows the CX3300 series to expand its application coverage from low-power IoT to mobile, automotive and various high current applications.
Thorough current profile evaluation of PDN devices is one of the most important measurements for IoT/mobile device characterization and validation. However, thorough evaluation takes a long time and requires complex setups because existing measurement instruments do not have enough capabilities to measure the current profile quickly and accurately.
Gaining a true picture of the current profile of mobile devices is important, due to the ever-increasing need for improved functionalities and performance, and also the need for lower power consumption.
Not having an effective solution for current profile measurement can cause the competitive advantage loss that can include:
The Keysight CX3300 is a solution that enables the characterization and validation of PDN for IoT/mobile devices quicker and more accurately. The ultra-low-noise, wide bandwidth and wide dynamic range performance of these new sensors (CX1104A and CX1105A), used with the CX3300 series now allows measurements at a wider range of dynamic current, from 1 μA to 100 A with more precision and speed.
Application example using these new sensors
Shown is the Keysight CX1104A Selectable Shunt Current Sensor and the Resistive Sensor Head
Shown is the Keysight CX1105A Ultra-Low Noise Differential SensorThe OS for the Keysight
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Magda Antone, Europe
+34 (93) 3434612
press.emea@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com