The Keysight nanoVTEP probe (E4333A) is the latest vectorless test solution from Keysight. The entire hardware assembly, including amplifier, has been miniaturized into a single probe, capable of performing vectorless testing on devices with a geometric outline as small as 4x4mm.
PCBAs in a fixture undergoing in-circuit test have hundreds, and up to thousands of test probes pressed against their electrical contact points. This generates a substantial amount of mechanical stress that is being countered by installing pressure fingers onto the fixture to minimize board flexing.
With denser board layouts, test engineers find it increasingly challenging to have sufficient clearance within the fixture to implement vectorless test techniques that detect open signal pins with capacitive coupling through a sensor plate.
Developed with advanced manufacturing techniques, Keysight’s nanoVTEP is 60% smaller compared to existing solutions in the market. Its small profile increases the opportunity to implement vectorless testing in a high-density fixture, thereby increasing coverage and fault detection rate in the test process
www.keysight.com/find/nanoVTEP
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Magda Antone, Europe
+34 (93) 3434612
press.emea@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com