The Keysight 5G mmWave non-signaling transceiver test solution validates multiple devices over the air quickly and repeatably. The compact, automated solution supports 28GHz and 39 GHz and uses reliable Keysight measurement science to accelerate 5G device validation and reduce cost of mmWave test.
Design and test at mmWave frequencies presents new challenges. Direct connections (like those used for testing devices today) do not provide an accurate representation of real-world conditions. Over-the-air (OTA) testing is required to validate devices with integrated mmWave antennas and ensure acceptance of designs. OTA testing can be expensive and time consuming, especially with the number of mmWave bands each design is expected to support.
Accurate and repeatable measurements are more challenging when performed over the air. To accurately validate broadband device performance, some measurements may need to be performed at intermediate frequencies (IF) in addition to RF.
To successfully scale mmWave device production cost effectively, lower cost mmWave design validation test solutions that support parallel test techniques are required.
Keysight has developed a simple solution to address these challenges. Multiple devices can be validated across multiple mmWave bands over the air using a compact solution employing familiar Keysight waveforms and measurements. Automation based on a universal Keysight platform provides chipset control and fast, reliable test results. A non-signaling test approach further speeds device validation. This 5G mmWave test solution accelerates device validation and reduces cost of test.
Figure 1: 5G mmWave non-signaling solution
Figure 2: EVM measurements
Figure 3: PAvT measurements
The Keysight 5G mmWave non-signaling test solution accelerates 5G device validation. A wideband transceiver provides access to IF and serves as the foundation for a flexible mmWave test solution. Test up to three device transmitters and receivers simultaneously with multiple RF and IF ports. The addition of one mmWave transceiver provides tunable access to the 28 GHz and 39 GHz bands defined by 3GPP. Add a chamber for testing over the air.
Validate device performance reliably using familiar Keysight waveforms and measurements. Flexibly create signals for custom and standards-based waveforms with Keysight Signal Studio software for 5G TF and 5G NR. Repeatably analyze device transmitters with Keysight X-Series Measurement applications for vector modulation analysis and 5G NR. Quickly validate RF performance with error vector magnitude (EVM), adjacent channel power (ACP), spectrum emission mask (SEM), power and occupied bandwidth (OBW) measurements along with IQ and spectrum analysis.
Test devices faster with automation based on the Keysight TAP platform providing powerful, flexible and extensible test sequence and test plan creation and optimizing software development and test performance. For faster characterization of mmWave antennas, Keysight has developed a measurement that captures and analyzes phase and amplitude components simultaneously (PAvT). Save even more time by testing without signaling.
With an OTA chamber, the solution provides a complete measurement environment for validating mmWave devices with integrated components and antennas. Performing typical OTA measurements such as total radiated power (TRP) and equivalent isotropically radiated power (EIRP) along with more typical RF measurements like EVM, power and ACP ensure mmWave devices are behaving as expected when used by consumers
For more information go to:
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Magda Antone, Europe
+34 (93) 3434612
press.emea@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com