What: |
The new Defining a Channel Sounding Measurement System for Characterization for 5G Air Interfaces application note offers insights into defining a channel sounding measurement system for characterization of 5G air interfaces using a variety of measurement methods. Keysight's 5G solutions help engineers gain greater insight into the standard as it continues to evolve. |
When: |
Available now. |
Where: |
The application note is available at www.keysight.com/find/5G-Insight. Registration is required. |
Additional |
# # #
Contacts:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com