[an error occurred while processing this directive] Images for Press Release

Agilent Technologies Introduces Industry's First Device Analyzer with Curve Tracer Functionality for Power-Device Evaluation

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

The Agilent B1505A Power Device Analyzer/Curve Tracer is the only single box solution available today with the capability to characterize devices at up to 3000 volts and 20 amps. The B1505A includes a curve tracer mode, which combines familiar curve tracer functionality with the convenience of a PC-based instrument, for improved ease of use and functionality for failure analysis of power device and power circuitry.

Image 1:
The Agilent B1505A Power Device Analyzer/Curve Tracer is the only single box solution available today with the capability to characterize devices at up to 3000 volts and 20 amps. The B1505A includes a curve tracer mode, which combines familiar curve tracer functionality with the convenience of a PC-based instrument, for improved ease of use and functionality for failure analysis of power device and power circuitry.

Download JPEG (0.6MB)

Download TIF (2.3MB)

 

Related Information
  Press Release:

Agilent Technologies Introduces Industry's First Integrated Product that Can Characterize All Modern Semiconductor Power Devices
(2012-May-01)

Agilent Technologies Introduces Industry's First Device Analyzer with Curve Tracer Functionality for Power-Device Evaluation
(2008-November-03)

  Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

  How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'