Agilent EXT Wireless Communications Test Set for Wireless Device Manufacturing

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

The Agilent EXT uses the proven X-Series Measurement Applications which simplify the creation of calibration and verification routines.

Image 1:
The Agilent EXT uses the proven X-Series Measurement Applications which simplify the creation of calibration and verification routines.

Low-JPEG Download (0.1MB)

High-JPEG Download (3.9MB)

The Agilent EXT offers a revolutionary high-speed measurement sequencer that gives the fastest approach to both calibration and verification of devices in manufacturing test.

Image 2:
The Agilent EXT offers a revolutionary high-speed measurement sequencer that gives the fastest approach to both calibration and verification of devices in manufacturing test.

Low-JPEG Download (0.1MB)

High-JPEG Download (3.9MB)

The Agilent Sequence Studio software application, exclusive to the EXT, dramatically reduces the time it takes to develop and troubleshoot the advanced fast-sequencing test code used in non-signaling test techniques.

Image 3:
The Agilent Sequence Studio software application, exclusive to the EXT, dramatically reduces the time it takes to develop and troubleshoot the advanced fast-sequencing test code used in non-signaling test techniques.

Low-JPEG Download (0.3MB)

Agilent EXT utilizes X-Series Measurement Applications and Sequence Studio software along with enhanced Signal Studio software to support the required testing of existing and emerging communication technologies such as LTE.

Image 4:
Agilent EXT utilizes X-Series Measurement Applications and Sequence Studio software along with enhanced Signal Studio software to support the required testing of existing and emerging communication technologies such as LTE.

Low-JPEG Download (0.2MB)

High-JPEG Download (5.0MB)

The Agilent EXT combined with the multiport adapter (MPA) provide cost effective multiport capability to increase throughput, reduce footprint per port, and lower the cost of test.

Image 5:
The Agilent EXT combined with the multiport adapter (MPA) provide cost effective multiport capability to increase throughput, reduce footprint per port, and lower the cost of test.

Low-JPEG Download (0.2MB)

High-JPEG Download (4.9MB)

The Agilent EXT-C with integrated multiport adapter provides reduced power consumption, reduced footprint, and effective utilization of test assets for lower cost of test.

Image 6:
The Agilent EXT-C with integrated multiport adapter provides reduced power consumption, reduced footprint, and effective utilization of test assets for lower cost of test.

Low-JPEG Download (0.1MB)

High-JPEG Download (9.6MB)

 

Related Information
  Press Release:

Agilent Technologies Announces Wireless Communications Test Set with Innovative Enhancements that Accelerate Manufacturing Test
(2012-August-1)

Agilent Technologies Signs Licensing Agreement with Qualcomm for Factory Test Technology (2011-February-16)

Agilent Technologies' Announces LTE Wireless Communications Test Set for Manufacturing (2011-February-14)

  Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

  How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'