Keysight FieldFox Handheld Analyzer Family
32/44/50 GHz FieldFox Microwave Analyzers N9950A/51A/52A
32/44/50 GHz FieldFox Spectrum Analyzers N9960A/61A/62A

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Image 1:
Keysight’s FieldFox is the industry’s first handheld combination analyzer to provide coverage to 50 GHz.

Low-JPEG Download (0.3MB)

High-JPEG Download (0.6MB)

Image 2:
Keysight’s FieldFox is the industry’s first handheld combination analyzer to provide coverage to 50 GHz.

Low-JPEG Download (0.3MB)

High-JPEG Download (0.6MB)

Image 3:
Keysight’s FieldFox is the industry’s first handheld combination analyzer to provide coverage to 50 GHz.

Low-JPEG Download (0.3MB)

High-JPEG Download (0.6MB)

Image 4:
Keysight FieldFox microwave analyzers provide unprecedented functionality and value at about half the cost of each equivalent benchtop instrument.

Low-JPEG Download (0.4MB)

High-JPEG Download (0.8MB)

Image 5:
Keysight FieldFox handheld analyzers provide more built-in capabilities than similar analyzers, and can replace three or four single-function instruments—benchtop or handheld—that are typically used for maintenance and troubleshooting of systems that operate at or above Ka-band frequencies.

Low-JPEG Download (0.3MB)

High-JPEG Download (0.6MB)

Image 6:
At only 7.1 pounds, the new Keysight FieldFox models deliver laboratory-grade measurements that enable field personnel to fully characterize today’s most demanding radar and satellite systems. Photo courtesy of INTELSAT.

Low-JPEG Download (0.7MB)

High-JPEG Download (1.4MB)

Image 7:
At only 7.1 pounds, the new Keysight FieldFox models deliver laboratory-grade measurements that enable field personnel to fully characterize today’s most demanding radar and satellite systems. Photo courtesy of INTELSAT.

Low-JPEG Download (0.7MB)

High-JPEG Download (1.3MB)

Image 8:
Verify the performance of microwave cables in the field easily with the portable Keysight FieldFox handheld analyzer. Photo courtesy of INTELSAT.

Low-JPEG Download (0.7MB)

High-JPEG Download (1.5MB)

Image 9:
The Keysight FieldFox analyzer is a rugged, dependable handheld designed to deliver precise, lab-grade measurements up to 50 GHz. Photo courtesy of INTELSAT.

Low-JPEG Download (1.0MB)

High-JPEG Download (2.1MB)

Image 10:
The Keysight FieldFox can be used to measure and verify waveguide components such as Ku band and Ka band

Low-JPEG Download (0.2MB)

High-JPEG Download (0.4MB)

Image 11:
In all six new Keysight FieldFox models, spectrum measurements are up to eight times faster than those made with comparable analyzers.

Low-JPEG Download (0.2MB)

High-JPEG Download (0.4MB)

Related Information

Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'