[an error occurred while processing this directive]

Introducing Agilent Technologies' Measurement Applications for the X-Series Signal Analyzers

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Image 1:
The new N9077A-4FP option supports the noncontiguous channel SEM of 80+80 MHz in 802.11ac on Agilent PXA, MXA and EXA X-Series signal analyzers.

Low-JPEG Download (0.4MB)

 

Image 2:
Agilent’s new WLAN list sequence capability (N9077A-5FP) speeds high-volume test by eliminating measurement switching and reconfiguration for disparate bursts. The displayed results (shown here for transmit power) can then be queried using SCPI commands.

Low-JPEG Download (0.2MB)

High-JPEG Download (0.3MB)

Image 3:
N9077A WLAN X-Series measurement application enhancements allow engineers to measure the full bandwidth of 802.11ac WLAN signals from 20 to 160 MHz and 80+80 MHz on Agilent’s highest performance PXA signal analyzer.

Low-JPEG Download (0.3MB)

 

Related Information
  Press Release:

Agilent Technologies Releases New Software for X-Series Signal Analyzers
(2012-November-01)

  Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

  How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'