Keysight BenchVue 3.5 Software

Keysight Technologies Announces BenchVue 3.5 Software for Instrument Control, Data Logging, Test Automation

Software Update Advances How Engineers Interact with Instruments and Entire Bench

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

BenchVue Software Icon.

Image 1:
BenchVue Software Icon.

Low-JPEG Download (0.1MB)

BenchVue is compatible with over 450 Keysight digital multimeters, power supplies, function generators, signal analyzers, network analyzers, oscilloscopes, power meters/sensors, FieldFox analyzers, signal generators, universal counters and data acquisition units.

Image 2:
BenchVue is compatible with over 450 Keysight digital multimeters, power supplies, function generators, signal analyzers, network analyzers, oscilloscopes, power meters/sensors, FieldFox analyzers, signal generators, universal counters and data acquisition units.

Low-JPEG Download (0.2MB)

High-JPEG Download (1.1MB)

Measurement View - See your measurements across instruments in one place to quickly correlate measurement activities and obtain actionable insight.

Image 3:
Measurement View - See your measurements across instruments in one place to quickly correlate measurement activities and obtain actionable insight.

Low-JPEG Download (0.2MB)

High-JPEG Download (1.1MB)

Capture - Depending on your measurement task, BenchVue provides extensive data, trace and measurement logging capabilities all from within one piece of software.

Image 4:
Capture - Depending on your measurement task, BenchVue provides extensive data, trace and measurement logging capabilities all from within one piece of software.

Low-JPEG Download (0.3MB)

High-JPEG Download (0.8MB)

Spectrum Analyzer app example.

Image 5:
Spectrum Analyzer app example.

Low-JPEG Download (0.3MB)

High-JPEG Download (0.8MB)

BenchVue Test Flow app is integrated into the BenchVue framework and occupies the right hand panel of the user interface.

Image 6:
BenchVue Test Flow app is integrated into the BenchVue framework and occupies the right hand panel of the user interface.

Low-JPEG Download (0.3MB)

High-JPEG Download (1.0MB)

BenchVue Test Flow app custom sequence example. Arrange the blocks in sequence in the order you want to run them. Top to bottom.

Image 7:
BenchVue Test Flow app custom sequence example. Arrange the blocks in sequence in the order you want to run them. Top to bottom.

Low-JPEG Download (0.2MB)

BenchVue app tab shows available apps for download, updating and licensing (NOTE: Some apps are installed by default and others can be added as needed by the user.)

Image 8:
BenchVue app tab shows available apps for download, updating and licensing (NOTE: Some apps are installed by default and others can be added as needed by the user.)

Low-JPEG Download (0.1MB)

High-JPEG Download (0.4MB)

Related Information
Benchview Software:

Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'