Agilent Technologies, PCI Express 3.0, N5393C, PCI Express, receiver test calibration and transmitter test software Option 004

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Product Images

The setup page for the RX calibration tool page

Image 1:
The setup page for the RX calibration tool page

Low-JPEG Download (0.2MB)

 

The setup page for the RX calibration tool page.

Image 2:
The setup page for the RX calibration tool page.

Low-JPEG Download (0.2MB)

High-JPEG Download (3.5MB)


PCI-SIG CBB3 Compliance Base Board (including riser), add-in card, and toggle circuit connection

Image 3:
PCI-SIG CBB3 Compliance Base Board (including riser), add-in card, and toggle circuit connection

Low-JPEG Download (0.4MB)

High-JPEG Download (4.3MB)

PCI-SIG x1/x16 CLB3 Compliance Load Board RX side.

Image 4:
PCI-SIG x1/x16 CLB3 Compliance Load Board RX side.

Low-JPEG Download (0.4MB)

High-JPEG Download (4.4MB)

PCI-SIG CBB3 Compliance Base Board w/o riser assembly (TX side).

Image 5:
PCI-SIG CBB3 Compliance Base Board w/o riser assembly (TX side).

Low-JPEG Download (0.3MB)

High-JPEG Download (4.1MB)

PCI-SIG CBB3 Compliance Base Board Riser Card (RX).

Image 6:
PCI-SIG CBB3 Compliance Base Board Riser Card (RX).

Low-JPEG Download (0.2MB)

High-JPEG Download (3.5MB)

PCI-SIG x1/x16 CLB3 Compliance Load Board RX side with toggle circuit connection.

Image 7:
PCI-SIG x1/x16 CLB3 Compliance Load Board RX side with toggle circuit connection.

Low-JPEG Download (0.3MB)

High-JPEG Download (4.0MB)

PCI-SIG x4/x8 CLB3 Compliance Load Board TX side.

Image 8:
PCI-SIG x4/x8 CLB3 Compliance Load Board TX side.

Low-JPEG Download (0.3MB)

High-JPEG Download (3.5MB)

Software Images

The N8816A Infiniium PCI Express 3.0 protocol analyzer software provides the ability to perform 128/130 bit and 8b/10b based packet decoding via a patented (patent pending) technique to capture and display serial data synchronized with the analog view of traffic of a serial data stream. Decode is displayed directly on the analog waveform as well as in the decode list with associated time and index displays. In conjunction with the decode list, using the multi-grid waveform display you can simultaneously display analog bi-directional waveforms with corresponding decode listings

Image 9:
The N8816A Infiniium PCI Express 3.0 protocol analyzer software provides the ability to perform 128/130 bit and 8b/10b based packet decoding via a patented (patent pending) technique to capture and display serial data synchronized with the analog view of traffic of a serial data stream. Decode is displayed directly on the analog waveform as well as in the decode list with associated time and index displays. In conjunction with the decode list, using the multi-grid waveform display you can simultaneously display analog bi-directional waveforms with corresponding decode listings.

Low-JPEG Download (0.4MB)

High-JPEG Download (0.5MB)

 

The expandable decode list provides an extendable indexed view of packet decode for users who are more accustomed to logic analyzer “vertical style” packet decode traffic listings.

Image 10:
The expandable decode list provides an extendable indexed view of packet decode for users who are more accustomed to logic analyzer “vertical style” packet decode traffic listings. The list includes color-coded packet types for easier visual searching of traffic patterns as well as a blue highlight that shows the packet that corresponds to the “blue line” in the waveform view.

Low-JPEG Download (0.4MB)

High-JPEG Download (0.6MB)

 

Related Information
  Press Release:

Agilent Technologies Introduces First Fully Integrated PCI Express® 3.0 Receiver Test Software
(2012-August-27)

  Press Release:

Agilent Technologies Introduces First Fully Integrated Protocol Viewer for Automated PCI Express® Testing
(2011-September-6)

  Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

  How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'