Agilent Technologies PXI Vector Signal Analyzer

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Image 1:
This image demonstrates the 3 channel set up. It consists of Agilent's M9362A-D01 four-channel downconverter, M9202A 12-bit digitizer, M9302A LO, M9168C RF attenuator, and the M9352A IF amplifier/attenuator modules in the Agilent PXIe (M9018A) chassis.

Low-JPEG Download (0.1MB)

High-JPEG Download (5.0MB)

 

Image 2:
This shows the PXI Vector Signal Analyzer dual-channel configuration with an embedded controller for RF interference detection and identification. The PXI modules that make up the solution are housed in the Agilent M9018A PXIe Chassis.

Low-JPEG Download (0.1MB)

High-JPEG Download (2.7MB)

 

 

Related Information
  Press Release:

Agilent Technologies Introduces the First Wideband, Dual-Channel PXI Vector Signal Analyzer with Streaming Capabilities for Detecting and Identifying RF Interference
(2012-April-03)

Agilent Technologies Introduces Industry's Widest-Bandwidth MIMO PXI Vector Signal Analyzer for Wireless Chipset Design and Verification
(2012-March-27)

  Video:

www.agilent.com/find/PXI-MIMOvideo

  Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

  How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'