The following product photos are available for use by the media, based on the Keysight Photography Use Policy.
Image 1:
Keysight 5G Testbed for Design Validation analyzing the performance of a phased array antenna in receive mode with a 3GPP NR signal in the presence of an unwanted interfering signal.
Low-JPEG Download (0.2MB)
High-JPEG Download (4.1MB)
Image 2:
An example measurement of a phased array antenna using 3GPP NR signals at 26 GHz achieving 1.1% EVM OTA.
Low-JPEG Download (0.2MB)
High-JPEG Download (1.0MB)
Image 3:
Shown is the Ball Aerospace / Anokiwave 26 GHz active antenna array innovator kit for 5G.
Low-JPEG Download (0.2MB)
High-JPEG Download (3.2MB)