Keysight Technologies' mmWave Testbed Enables Ball Aerospace, Anokiwave to Validate First Commercial 5G NR Active Array Antenna Designs at 26 GHz

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Keysight 5G Testbed for Design Validation analyzing the performance of a phased array antenna in receive mode with a 3GPP NR

Image 1:
Keysight 5G Testbed for Design Validation analyzing the performance of a phased array antenna in receive mode with a 3GPP NR signal in the presence of an unwanted interfering signal.

Low-JPEG Download (0.2MB)

High-JPEG Download (4.1MB)

An example measurement of a phased array antenna using 3GPP NR signals at 26 GHz achieving 1.1 percent EVM OTA

Image 2:
An example measurement of a phased array antenna using 3GPP NR signals at 26 GHz achieving 1.1% EVM OTA.

Low-JPEG Download (0.2MB)

High-JPEG Download (1.0MB)

The Ball Aerospace, Anokiwave 26 GHz active antenna array innovator kit for 5G

Image 3:
Shown is the Ball Aerospace / Anokiwave 26 GHz active antenna array innovator kit for 5G.

Low-JPEG Download (0.2MB)

High-JPEG Download (3.2MB)

Related Information

Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'