The Keysight N5291A broadband millimeter-wave network analyzer and PNA Series network analyzers

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Keysight N5291A broadband millimeter wave network analyzer

Image 1:
The Keysight N5291A broadband millimeter-wave network analyzer enables developers to confidently characterize new-generation designs.

Low-JPEG Download (0.2MB)

High-JPEG Download (0.4MB)

Keysight N5291A broadband millimeter-wave network analyzer wafer measurements

Image 2:
In this configuration, a four-port Keysight N5291A broadband millimeter-wave network analyzer is being used to perform on-wafer measurements of a differential amplifier.

Low-JPEG Download (0.2MB)

Keysight PNA and PNA-X families of network analyzers touch based UI

Image 3:
Keysight's PNA Series network analyzers now feature a touch-based user interface that includes task-specific guides such as this "millimeter configuration" screen, thereby helping new or infrequent users achieve better results in less time.

Low-JPEG Download (0.2MB)

High-JPEG Download (0.5MB)

Related Information

Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'