SANTA ROSA, Calif., Oct. 1, 2014
Keysight Technologies, Inc. today announced the M9188A, a PXI-based, 16-channels, single-slot unipolar dynamic digital/analog converter (DAC). The M9188A is capable of supplying typical waveforms of up to +30 V. This eliminates the need for engineers to design and develop signal conditioning circuits for applications requiring up to +30 V and thus reduces test system application development and setup time.
The M9188A provides a variable current source, such as DC, and pulse waveforms of up to +20 mA. This eliminates the need for an additional current transformer or source measure unit for application tests requiring current source signals. This helps users achieve a lower cost of test resulting in lower capital expenditure requirements.
The M9188A has an output disconnect switch at every channel. This helps prevent potential damage to the device under test (DUT) from external signal power sources and helps user achieve greater uptime.
With 1 MB available memory per channel, the M9188A can behave like a basic arbitrary waveform generator (ARB) by simulating waveforms with a sampling period from 2 μs to 512 μs at up to 500 kSa/s update rate.
The M9188A is ideal for:
U.S. Pricing and Additional Information
The M9188A is available today with prices starting at $3,600. More information is available at www.keysight.com/find/m9188a or contact Keysight Technologies. Images of the M9188A are available at www.keysight.com/find/m9188a_images.On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.
Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.
Forward-Looking Statements
This news release contains forward-looking statements as defined in the Securities Exchange Act of 1934 and is subject to the safe harbors created therein. The forward-looking statements contained herein include, but are not limited to, information regarding Keysight's separation of the electronic measurement business; future revenues, earnings and profitability; the future demand for the company's products and services; and customer expectations. These forward-looking statements involve risks and uncertainties that could cause Keysight's results to differ materially from management's current expectations. Such risks and uncertainties include, but are not limited to, unforeseen changes in the strength of our customers' businesses; unforeseen changes in the demand for current and new products, technologies, and services; customer purchasing decisions and timing, and the risk that we are not able to realize the savings expected from integration and restructuring activities.
In addition, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10, and amendments thereto. Forward-looking statements are based on the beliefs and assumptions of Keysight's management and on currently available information. Keysight undertakes no responsibility to publicly update or revise any forward-looking statement.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com