Keysight Technologies Announces Expanded TRX Module and EXM Wireless Test Set Enhancements

  
  

New Module Helps Manufacturers Achieve Maximum Production Throughput

SANTA ROSA, Calif., Oct. 2, 2014

Keysight Technologies, Inc. today announced the market's first TRX module with four full-duplex RFIO ports and other firmware enhancements for the E6640A EXM wireless test set. The TRX module sets a new industry standard, allowing manufacturers to test up to four connected devices with identical RFIO performance and therefore achieve maximum production throughput.

Keysight also announced today new EXM enhancements including 1) advanced sequencing of multiple WLAN formats within one test sequence to enable faster WLAN device production test; and 2) speed-optimized firmware to help manufacturers enhance wireless device test plan efficiency and increase production throughput. The addition of DECT, PHS and Zigbee support adds to the EXM's already long list of multi-format measurement capabilities.

"Cellular and WLAN device manufacturers need a high-port-density test solution to meet the growing demand for wireless devices with multiple radios and antennas," stated Joe DePond, vice president and general manager of Keysight's Mobile Broadband Operation. "The EXM gives manufacturers a platform that protects their investment and easily evolves with our customers' changing needs on the production floor."

As wireless chipset vendors and device manufacturers continue to move forward with fast-sequenced non-signaling test, the EXM continues to fill the need for faster test execution. The recent signed manufacturing test license (MTL) agreement with Broadcom Corporation is one of the examples of Keysight's commitment to solving today's customer problems and tomorrow's challenges with new core features and capabilities. The EXM features:

  • Up to four independent TRX modules supporting up to 16 connections without the use of external fixtures or switching.
  • Multi-format measurement application support including LTE/LTE-Advanced, HSPA+, W-CDMA, cdma2000®, GSM/EDGE/Evo, TD-SCDMA, PHS, DECT, WLAN 802.11 a/b/g/n/j/p/ac, Bluetooth® BR/EDR/LE, GNSS (GPS, GLONASS, Galileo, Bei Dou, QZSS), Mobile WiMAX™, Zigbee, PHS, and digital video.
  • Independent source and analyzer on each TRX.
  • Four RF ports configured as two full-duplex and two half-duplex ports or four full–duplex ports.
  • Support for up to 32 devices-under-test through customizable multi-port adapter (MPA) technology.
  • 160-MHz bandwidth, up to 6-GHz frequency range, best-in-class ±0.2 dB power-level accuracy at 3.8 GHz, and -43 dB receiver EVM noise floor for 802.11ac.

Additional Information

 Product information is available at www.keysight.com/find/exm. High-resolution images are available at www.keysight.com/find/exm_images. Contact Keysight for additional information and pricing.
About Keysight Technologies

On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.

Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.

Forward-Looking Statements

This news release contains forward-looking statements as defined in the Securities Exchange Act of 1934 and is subject to the safe harbors created therein. The forward-looking statements contained herein include, but are not limited to, information regarding Keysight's separation of the electronic measurement business; future revenues, earnings and profitability; the future demand for the company's products and services; and customer expectations. These forward-looking statements involve risks and uncertainties that could cause Keysight's results to differ materially from management's current expectations. Such risks and uncertainties include, but are not limited to, unforeseen changes in the strength of our customers' businesses; unforeseen changes in the demand for current and new products, technologies, and services; customer purchasing decisions and timing, and the risk that we are not able to realize the savings expected from integration and restructuring activities.

In addition, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10, and amendments thereto. Forward-looking statements are based on the beliefs and assumptions of Keysight's management and on currently available information. Keysight undertakes no responsibility to publicly update or revise any forward-looking statement.

# # #

cdma2000 is a US registered certification mark of the Telecommunications Industry Association. 

Bluetooth is a trademark owned by Bluetooth SIG, Inc., U.S.A. and licensed to Keysight Technologies, Inc.

Mobile WiMAX is a US trademark of the WiMAX Forum.