Agilent Technologies' 80- and 120-MHz Trueform Waveform Generators Deliver Unrivaled Capabilities and Signal Accuracy

  
  

Instruments Offer Lowest Jitter, Lowest Harmonic and Non-Harmonic Distortion in Class

SANTA CLARA, Calif., March 3, 2014

Agilent Technologies Inc. (NYSE: A) today introduced the 33600A Series waveform generators with exclusive Trueform signal-generation technology. With Trueform, the instruments are able to deliver unmatched capabilities used to generate a full range of signals for even the most demanding measurements required by engineers and technicians during electronic device design and manufacturing test.

Agilent's 33600A Series, which comprises four different one- and two-channel models, can generate waveforms up to 120 MHz at a 1 GSa/s sampling rate. The waveform generators provide the lowest jitter (less than 1 ps jitter, or 200x better than previous generation Direct Digital Synthesis generators) and lowest total harmonic distortion in their class, giving engineers the ability to generate the exact signals they need. Better jitter performance means that technicians and engineers can place edges more accurately, which helps them reduce timing errors in their circuit designs. With total harmonic distortion less than 0.03 percent and non-harmonic spurs below -75 dBc, the 33600A Series offers clean signals that don't introduce noise, enabling users to get more accurate results.

The 33600A Series' very low jitter and 3-ns rise and fall times also allow users to set trigger points more accurately. A low voltage range, 1 mVpp, enables them to make output changes down to 1 µV-a critical capability when testing today's low-voltage circuits and designs.

As an added benefit, 33600A Series users can take advantage of easy software upgrades to expand their instruments' capabilities, such as when they need to increase memory to 64 MSa or bandwidth to 120 MHz, for example. They can even upgrade their instruments to NISPOM file security.

Trueform Technology

While traditionally DDS has been the waveform-generation technology of choice, its intrinsic limitations mean users often have to work around its compromised performance or spend up to five times more for a high-end waveform generator. Trueform technology eliminates these challenges by combining the best of DDS with a point-per-clock architecture. When used in the 33600A Series, the results are a range of capabilities not normally found on waveform generators in this class, including:

  • Waveform summing and combining for easily adding noise to signals for margin and distortion testing using only a single channel. On the two-channel 33600A Series model users can sum and combine up to four signals.
  • Variable-bandwidth noise for adjusting the bandwidth of the built-in noise generator to control a signal's frequency content.
  • Waveform sequencing for creating multiple configured waveforms with several common segments and building long, complex waveforms using minimal instrument memory.
  • Pseudo-Random Binary Sequence (PRBS) pattern generation for testing digital serial buses by streaming standard PRBS patterns-with PN3 to PN32-without a separate pulse generator.
  • Optional baseband IQ player for wireless communication engineers wanting to economically play IQ signals without an expensive signal generator, or make adjustments (e.g., amplitude gain, channel offset and channel skew) to the signal, as needed, for a more accurate representation.

"Trueform technology represents a revolutionary change in waveform generation from previous techniques such as DDS," said Huei Sin Ee, vice president and general manager of Agilent's General Purpose Electronics Measurement Division. "Using an exclusive digital sampling technique, it is able to deliver unmatched performance and superior signal fidelity at the same low price customers expect with DDS. Thanks to these capabilities, our new 33600A Series Trueform waveform generators are now enabling technicians and engineers to dramatically accelerate development of even their most complex waveforms."

U.S. Pricing and Availability

Agilent's new 33600A Trueform Series waveform generators are available now. Pricing is as follows:

33611A 1-channel, 80 MHz $3,995
33612A 2-channel, 80 MHz $5,695
33621A 1-channel, 120 MHz $4,695
33622A 2-channel, 120 MHz $6,695

More information on the 33600A Series is available at www.agilent.com/find/33600A. Images of the waveform generators are available at www.agilent.com/find/33600A_images. For a video highlighting the new 33600A Series' key features, go to www.agilent.com/find/33600A_video. A backgrounder on Trueform technology is available at www.agilent.com/find/33600A_backgrounder.


About Agilent Technologies

Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.

On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent

Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com