SANTA CLARA, Calif., March 4, 2014
Agilent Technologies Inc. (NYSE: A) today announced the introduction of the M9393A PXIe performance vector signal analyzer (VSA), offering speed and accuracy previously unseen in modular instrumentation, up to 27 GHz. The M9393A delivers Agilent's proven microwave measurement technology in a PXI form-factor for manufacturing and design validation of transmitters and components for radar, military, satellite and commercial wireless communications.
The innovative design of the M9393A offers engineers the ability to validate the true performance of leading-edge and legacy devices with frequency coverage from 9 kHz to 27 GHz and 160 MHz analysis bandwidth. In addition to excellent performance-including ±0.15 dB absolute amplitude accuracy, -160 dBm displayed average noise level (DANL), with preamplifier, and +30 dBm third-order intermodulation (TOI)-the M9393A delivers frequency switching in less than 150 microseconds, dramatically reducing test time to increase throughput.
"The introduction of the M9393A is the culmination of close collaboration between our customers and development teams to provide a breakthrough in microwave signal analysis," said Agilent's Mark Pierpoint, vice president and general manager, Modular Solutions Division. "Not only does the PXI form-factor give system-ready capability for single or multi-channel measurements in a small footprint, but it also delivers unmatched speed and the confidence in measurement results that come only with Agilent's industry-proven measurement science."
The M9393A leverages Agilent's highly regarded X-Series measurement applications and 89600 VSA software, which offers deep programmatic compatibility with Agilent's benchtop signal analyzers to maximize test code reuse. It provides consistent, accurate results across instrument form-factor and product lifecycle. The 89600 VSA software's new stepped spectrum capability allows the M9393A to measure across 27 GHz in less than 1 second, with 10 kHz resolution bandwidth, for fast measurements of harmonics and spurs. The X-Series measurement applications for modular instruments can be used with the M9393A to simplify device conformance testing for LTE, WLAN and more.
Beyond the inherent flexibility and scalability of PXI, the M9393A is designed for extensibility. License-key upgradeable options for frequency, analysis bandwidth, preamplifiers and memory allow engineers to easily adapt to changing test needs with quick system updates. The truly modular architecture of the M9393A means that as hardware advances, a single module's upgrade or replacement maximizes reuse of existing equipment and dramatically reduces the cost of test.
Using the new Agilent M9037A PXI embedded controller, the M9393A measurement capability speed is increased. A high-performance PC computer designed for complex or multi-chassis systems and secure environments, the M9037A features a 2.4 GHz quad-core processor with up to 12 GB/s data bandwidth. The high-speed CPU is based on the Intel i7 4700EQ and adds the advantage of fast computation speeds such as needed for EVM and power measurements, thus decreasing test time and increase throughput.
U.S. Pricing and Availability
The M9393A is now available for order and will ship in July. The list price is from $42,000.
More information is available at www.agilent.com/find/M9393A. High-resolution images are available at www.agilent.com/find/M9393A_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com