SANTA ROSA, Calif., Sept. 10, 2014
Keysight Technologies, Inc. today announced the E6650A EXF wireless test set, the industry's first one-box tester dedicated to femtocell manufacturing. The EXF delivers the speed, performance and scalability needed to ramp up production and lower the cost of test. Validation with the latest cellular and WLAN chipsets reduces start-up time.
The EXF reduces overall test time through hardware and software elements optimized for speed. Each unit can be configured with up to four transmit/receive (TRX) modules, each of which is a complete vector signal analyzer and vector signal generator (VSA/VSG). In addition, each TRX has two full-duplex and two half-duplex ports, enabling users to create high-density multi-port test stations.
A multi-channel EXF can test multiple devices-under-test and supports the use of parallel, sequential and hybrid methods in a single chassis. Capabilities such as advanced sequencing and single-acquisition multiple measurements (SAMM) further reduce test time.
"As small cells gain momentum, keeping pace with growing demand and aggressive schedules is easier with access to deeper knowledge," said Satish Dhanasekaran, marketing manager of Keysight's Microwave and Communications Division. "With our expertise in the testing of high-performance base stations and high-volume user devices, local Keysight application specialists can fine-tune the EXF to help manufacturers accelerate time-to-volume in femtocell manufacturing."
To meet the testing needs of multi-format designs, the EXF supports 2G, 3G, 4G and WLAN with frequency coverage up to 6 GHz and bandwidth of up to 160 MHz in each TRX. Specific formats include LTE FDD, LTE TDD, and more, in cellular, and 802.11a, b, g, n and ac in WLAN. As requirements change, the ability to upgrade capabilities such as frequency range and channel count ensures easy evolution and investment protection.
Because Keysight has validated the EXF with leading cellular and WLAN chipsets, femtocell manufacturers can quickly ramp up from product introduction to volume manufacturing. To simplify test automation, the EXF includes standardized SCPI commands and reference drivers.
For faster test migration, the EXF is compatible with the Keysight X-Series signal analyzers and signal generators commonly used in R&D. Because the EXF uses the same X-Series measurement applications, it delivers repeatable results that enable a seamless transition to manufacturing.
The E6650A EXF wireless test set for femtocells is available now.
More information is available online at www.keysight.com/find/EXF. High-resolution product images can be downloaded from www.keysight.com/find/EXF_images.
On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.
Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.
Forward-Looking Statements
This news release contains forward-looking statements as defined in the Securities Exchange Act of 1934 and is subject to the safe harbors created therein. The forward-looking statements contained herein include, but are not limited to, information regarding Keysight's separation of the electronic measurement business; future revenues, earnings and profitability; the future demand for the company's products and services; and customer expectations. These forward-looking statements involve risks and uncertainties that could cause Keysight's results to differ materially from management's current expectations. Such risks and uncertainties include, but are not limited to, unforeseen changes in the strength of our customers' businesses; unforeseen changes in the demand for current and new products, technologies, and services; customer purchasing decisions and timing, and the risk that we are not able to realize the savings expected from integration and restructuring activities.
In addition, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10, and amendments thereto. Forward-looking statements are based on the beliefs and assumptions of Keysight's management and on currently available information. Keysight undertakes no responsibility to publicly update or revise any forward-looking statement.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com