SANTA ROSA, Calif., Oct. 20, 2014
Keysight Technologies, Inc. today introduced CAN FD (controller area network with flexible data-rate) and SENT (single-edge nibble transmission) decoding and triggering options for its InfiniiVision 4000 X-Series oscilloscopes. The new capabilities improve engineers’ efficiency in debugging CAN FD and SENT serial buses, which are used primarily in automotive applications.
CAN FD is the next-generation, higher-performance serial bus protocol for automotive control and diagnostic applications. It allows engineers to reduce bus loads and increase throughput for today’s demanding automotive applications. With “classic” CAN 2.0, transmission rates are limited to 1 Mbps because of the event-driven nature of this serial bus. With CAN FD, transmission rates increase during the data phase of each frame and maximum specified payload sizes are increased from 8 bytes up to 64 bytes. Moving from CAN 2.0 to CAN FD technology offers an easier and more seamless migration path compared with adopting other time-triggered serial bus protocols such as FlexRay.
With the higher data rates of CAN FD, using an oscilloscope to test and debug the signal integrity (physical layer) of these higher-speed signals is critical. Keysight’s new CAN FD triggering and decode capabilities in the InfiniiVision 4000 X-Series oscilloscopes rely on hardware-based decoding to enable the industry’s fastest decode update rates. Faster waveform and decode update rates increase the scope’s probability of capturing random and infrequent errors. Detection and elimination of bus errors during the design phase is crucial for automotive safety.
In addition to the ability to quickly capture infrequent bus errors with hardware-based decoding, 4000 X-Series oscilloscopes provides the industry’s most extensive CAN FD error triggering and analysis. This includes the ability to decode, totalize, and trigger on specific errors (optionally filtered by frame ID) such as stuff bit errors, form errors, CRC errors, acknowledge errors, and error frames.
SENT is a point-to-point serial bus that interfaces sensors to ECUs. Keysight’s new SENT option for InfiniiVision 4000 X-Series oscilloscopes provides decoding for serial data on fast and slow channels and offers extensive triggering selections, including the ability to trigger on various error conditions. The InfiniiVision 4000 X-Series is the only oscilloscope available today that can trigger on SENT bus signals.
Additional information about CAN FD and SENT options for the InfiniiVision 4000 X-Series oscilloscopes is available at www.keysight.com/find/scopes-auto. Product images are available at www.keysight.com/find/DSOX4AUTO_images.
Keysight’s complete oscillos cope portfolio includes instruments with a variety of form factors with bandwidths from 20 MHz to 90 GHz.
The CAN FD version 1.0 specification from Robert Bosch GmbH is available at www.bosch-semiconductors.de/media/pdf_1/canliteratur/can_fd_spec.pdf.
The SENT specification (SAE J2716) from SAE International is available at www.sae.org.
U.S. Pricing and Availability
The DSOX4AUTO option for CAN, CAN-dbc, CAN FD and LIN triggering and decoding is priced at $1,530. Customers who already own a Keysight 4000 X-Series oscilloscope with the DSOX4AUTO option can upgrade their oscilloscopes at no charge with the latest firmware to enable CAN FD support.
The DSOX4SENSOR option for SENT triggering and decoding is priced at $1,530.
The entry-level price of a Keysight InfiniiVision 4000 X-Series oscilloscope licensed with either of these new options is $7,150.
All of these products are available now.
On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.
Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.
Forward-Looking Statements
This news release contains forward-looking statements as defined in the Securities Exchange Act of 1934 and is subject to the safe harbors created therein. The forward-looking statements contained herein include, but are not limited to, information regarding Keysight's separation of the electronic measurement business; future revenues, earnings and profitability; the future demand for the company's products and services; and customer expectations. These forward-looking statements involve risks and uncertainties that could cause Keysight's results to differ materially from management's current expectations. Such risks and uncertainties include, but are not limited to, unforeseen changes in the strength of our customers' businesses; unforeseen changes in the demand for current and new products, technologies, and services; customer purchasing decisions and timing, and the risk that we are not able to realize the savings expected from integration and restructuring activities.
In addition, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10, and amendments thereto. Forward-looking statements are based on the beliefs and assumptions of Keysight's management and on currently available information. Keysight undertakes no responsibility to publicly update or revise any forward-looking statement.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com