SANTA ROSA, Calif., Sept. 1, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today added six millimeter-wave models to its family of FieldFox handheld analyzers. The flagship model is the industry’s first handheld combination analyzer to provide coverage to 50 GHz. With more built-in capabilities than similar analyzers, FieldFox can replace three or four single-function instruments — benchtop or handheld — that are typically used for maintenance and troubleshooting of systems that operate at or above Ka-band frequencies.
"At only 7.1 pounds, the new FieldFox models deliver laboratory-grade measurements that enable field personnel to fully characterize today’s most demanding radar and satellite systems," said Dan Dunn, general manager for RF and microwave handheld analyzers. "In addition, a FieldFox combination analyzer provides unprecedented functionality and value at about half the cost of each equivalent benchtop instrument."
Three combination-analyzer models cover 32, 44 or 50 GHz and provide spectrum analysis, vector network analysis and cable and antenna testing in a rugged, portable unit. The three spectrum analyzer models cover the same frequency range.
In all six new models, spectrum measurements are up to eight times faster than those made with comparable analyzers. FieldFox millimeter-wave analyzers are also three pounds lighter than similar units from other vendors.
The FieldFox family is optimized for field testing. The fully sealed enclosure — no fans or vents — is compliant with US MIL-PRF-28800F Class 2 standards and is also type tested to meet MIL-STD-810G requirements for operation in explosive environments (Method 511.5, Procedure 1). FieldFox analyzers are also type tested to meet IEC/EN 60529 IP53 requirements for protection from dust and water.
The analyzers offer a broad array of functionality that is software upgradeable, enabling users to choose the capabilities they need initially and add others later. Examples include vector voltmeter, TDR cable measurements, built-in power meter, pulse measurements, spectrum analyzer time gating, interference analyzer (with spectrogram), and GPS receiver.
U.S. Pricing and Availability
All six models are available now:
Pricing starts at $28,000 for the N9950A 32 GHz FieldFox microwave combination analyzer.
More information is available at www.keysight.com/find/first50. Images are available at www.keysight.com/find/FieldFox_first50_images. The following FieldFox backgrounders are available:
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers’ measurement experience through innovations in wireless, modular, and software solutions. Keysight’s electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]