SANTA ROSA, Calif., Sept. 3, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced the industry's highest performance PXIe multiport vector network analyzer, the M9485A VNA, designed for high-volume wireless component manufacturing of front-end modules, switches and filters used in mobile phones and base stations.
The true multiport architecture provides best-in-class measurement speed up to 30 percent faster than competing offerings, while maintaining high dynamic range. Frequency coverage of 1 MHz to 9 GHz is suitable for future component designs. Customers can configure exactly the port count they need, saving money and enabling fast re-configuration as test needs change.
During volume manufacturing, test speed is critical and space is often limited. With its true multiport capability up to 24 ports, all receivers synchronize with a common source to measure all S-parameters at once. When measuring multiport devices, this configuration drastically reduces the sweep time as compared to a switch matrix-based solution. These capabilities speed test by improving both productivity and throughput, while also minimizing space.
"A true multiport PXI VNA provides higher throughput with fewer sweeps than a VNA with a switch matrix for the same multiport device," said Akira Nukiyama, vice president and general manager, Keysight's Component Test Division, Kobe. "For example, with our 24-port PXIe VNA, a 24-port device only requires 24 sweeps versus 264 sweeps with a 4-port VNA and a switch matrix. That reduces sweep time more than 10 times, and there is no degradation in performance."
The new M9485A PXIe multiport VNA provides the industry's best performance with a fast speed (5 msec at 201 points with 2-port calibration) and wide dynamic range (up to 142 dB dynamic range). The VNA also delivers low trace noise (0.001-dBrms at 10 kHz IFBW) and high stability (0.005 dB/°C). When coupled with the M9485A's multiport and multi-site measurement capabilities, this level of performance helps decrease the cost of test.
Keysight's new multiport PXIe VNA supports a frequency offset mode, time domain analysis, and N-port calibrated measurements based on the same measurement science and calibration science as trusted PNA/ENA network analyzers. By using the PXI module concept, the VNA allows users to perform flexible upgrade and repair as necessary. Users also gain significant space savings as compared to bench-top type instruments with an equivalent number of ports.
U.S. Pricing and Availability
The M9485A PXIe multiport VNA is available now worldwide. A 12-port configuration of the VNA is available for $120,000, while a 24-port configuration is available for $197,000 (including the M9018A PXIe chassis and M9037A controller).
More information on the M9485A VNA is available at www.keysight.com/find/m9485a. An image of the new VNA is available at www.keysight.com/find/M9485A_images.
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]