SANTA ROSA, Calif., Jan. 7, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today announced that its N9038A MXE EMI receiver is now available with a frequency range of 20 Hz to 3.6 GHz. The affordable pricing of this new option addresses the needs of commercial manufacturers that perform compliance testing in their own facilities and do not require measurements at higher frequencies.
Electromagnetic compatibility (EMC) compliance testing is required for all electronic products and is regulated by a variety of agencies around the world. Example applications in the 3.6 GHz range include automotive, industrial, scientific, medical, consumer and "Internet of Things" (IoT) products.
Designed specifically for EMC testing, the MXE EMI receiver is compliant with the world's two major sets of requirements: CISPR 16-1-1 for commercial products and MIL-STD-461 for military systems. With the new option, test engineers can configure the MXE with a frequency range of 20 Hz to 3.6, 8.4, 26.5, or 44 GHz.
"In the lab and on the bench, the MXE provides the accuracy, repeatability and reliability self-certifiers need to test automotive and IoT products," said Satish Dhanasekaran, marketing manager of Keysight's Microwave and Communications Division. "With its built-in spectrum analysis capabilities, the 3.6 GHz MXE helps reduce the cost of test and also enables EMI/EMC specialists to diagnose noncompliant emissions and help designers pinpoint the root causes."
Built on an upgradeable platform, the MXE enables test labs to keep the instrument current and extend its longevity. Available enhancements include CPU, memory, disk drives and I/O ports. Users can also add functionality and measurement applications through simple license key upgrades.
U.S. Pricing and Availability
The 3.6 GHz N9038A MXE EMI receiver is available now at a base price of $61,000.
More information is available online at www.keysight.com/find/MXE. High-resolution product images are available at www.keysight.com/find/MXE_images.Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com