SANTA ROSA, Calif., July 7, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced a BGA (ball grid array) interposer solution for testing DDR4 x16 DRAM (dynamic random access memory) designs with a logic analyzer. Using the Keysight W4636A DDR4 x16 BGA interposer solution, engineers can quickly and accurately capture address and command signals, and a subset of data signals, for debugging designs and performing functional validation measurements for data rates up to 2,400 Mb/s.
The Keysight W4636A BGA interposer is the world's smallest DDR4 x16 BGA interposer solution for use with a logic analyzer, making it ideal for testing designs with tight space restrictions.
As the memory industry transitions to DDR4 designs, engineers working on next-generation memory systems – such as those used in servers and embedded devices – face significant challenges. Probing and accurate signal capture are becoming increasingly critical for debug and validation of new designs. The W4636A DDR4 x16 two-wing, small-KOV (keep-out volume), BGA interposer – the latest addition to the W4630A Series DDR4 BGA interposer family – is for engineers who need to view DDR4 x16 DRAM traffic and have limited KOV on their systems under test. It is also for engineers who need to perform functional compliance tests on DDR4 devices with ADD/CMD signals.
The W4636A interposer solution provides direct access to the balls of JEDEC-standard DDR4 x16 96-ball DRAM with low loading and minimal impact to signal integrity on embedded-system designs. The interposer solution is designed to be used with the Keysight U4154B logic analysis system, E5847A ZIF (zero insertion force) probes and U4201A cables for functional compliance and performance validation and analysis on ADD/CMD and a subset of DQ (data).
"Our customers need a selection of DDR4 BGA interposers to cover a variety of system designs," said David Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "With the W4636A interposer and U4154B logic analyzer system, engineers with tight space restrictions are ready to test DDR4 x16 DRAM in their systems."
For engineers who require access to all ADD/CMD/DQ/DQS at data rates more than 2,400 Mb/s, the W4633A x4/x8 DDR4 BGA interposer and W4631A x16 DDR4 BGA interposers capture all ADD/CMD/DQ/DQS signals at data rates of at least 3.2 Gb/s.
The U4154B logic analysis module with 4-Gb/s state speed enables engineers to reliably trigger on specific events and capture DDR4 traffic. When used with the new DDR4 interposer solutions, B4621B DDR decoder and B4622B compliance software toolset, this module provides functional test capability for system integration in the memory industry with visibility of the upper data byte lane up to 2,400 Mb/s.
Additional information about Keysight's W4636A DDR4 x16 BGA interposer can be found at www.keysight.com/find/W4636A. Product images are available at www.keysight.com/find/W4636A_images.
Keysight offers a complete logic analyzer portfolio of instruments with a variety of form factors to meet customer needs.
U.S. Pricing and Availability
The Keysight W4636A DDR4 x16 DRAM interposer solution can be ordered now with prices starting at $1,500.
Complete U4154B logic analyzer systems for probing DDR4 DRAM at 2.4 Gb/s start at $133,000.
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com