Keysight Technologies Introduces First Mainstream Oscilloscopes with Capacitive Touch Screens, Zone Triggering

  
  

Intuitive Graphical Triggering Helps Engineers Solve Problems Faster, Improve Productivity

SANTA ROSA, Calif., Jan. 8, 2015

Keysight Technologies, Inc. (NYSE: KEYS) today introduced InfiniiVision 3000T X-Series digital-storage and mixed signal oscilloscopes with intuitive graphical triggering capability. This new oscilloscope series delivers capacitive touch screens and zone triggering to the mainstream oscilloscope market for the first time. The scopes help engineers overcome usability and triggering challenges and improve their problem-solving capability and productivity.

As digital speeds and device complexity continue to increase, signals under test are getting more complex, and engineers are more challenged to isolate anomalies in their devices. Intuitive graphical triggers, previously unavailable in mainstream oscilloscopes, help engineers debug and characterize their cutting-edge devices faster and more easily. With graphical triggers, engineers can use a finger to draw a box around a signal of interest on the instrument display to create a trigger.

The new oscilloscope series offers upgradable bandwidths from 100 MHz to 1.0 GHz and several benchmark features in addition to the touch screen interface and graphical zone triggering capability. An uncompromised update rate of one million waveforms per second gives engineers visibility into subtle signal details. The series comes with six-instruments-in-one integration, including oscilloscope functionality, digital channels (MSO), protocol analysis capability, a digital voltmeter, a WaveGen function/arbitrary waveform generator, and an 8-digit hardware counter/totalizer. Finally, the 3000T X-Series delivers correlated frequency and time domain measurements using the gated FFT function for the first time in this class, to address emerging measurement challenges.

"These new scopes give engineers using mainstream oscilloscopes an uncompromised ability to find and isolate the most difficult problems in their designs," said Dave Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "Design-for-touch operation improves their debugging efficiency. Mixed-domain analysis capabilities with time-correlated frequency/time domain measurements, six-in-one integration and a rich set of advanced features accelerate their problem solving."

The 3000T X-Series was designed specifically for operation with a capacitive touch screen, which allows engineers to select targets naturally and quickly. To further improve productivity, the interface includes an alphanumeric touchpad that replaces tedious knob-based operation and touch-based interaction that enables greater flexibility in displaying measurement information.

With the series' uncompromised high-speed waveform update rate, even with the digital channel, protocol decode, measurements and math functions turned on and simplicity of zone touch triggering, engineers have the highest probability of discovering anomalies of interest.

The 3000T X-Series supports a wide range of popular and emerging serial bus applications: MIL-STD 1553 and ARINC 429, I2S, CAN/CAN-FD/CAN-Symbolic, LIN, SENT, FlexRay, RS232/422/485/UART and I2C/SPI. The new gated FFT function allows engineers to correlate time and frequency domain phenomenon on a single screen. Finally, the power analysis, video analysis and hardware-based mask test option makes the 3000T X-Series a comprehensive mainstream oscilloscope.

The InfiniiVision 3000T X-Series includes 100-MHz, 200-MHz, 350-MHz, 500-MHz and 1-GHz models. The standard configuration for all models includes 4 Mpts of memory, segmented memory, advanced math and 500-MHz passive probes.

U.S. Pricing and Availability

Keysight InfiniiVision 3000T X-Series oscilloscopes are available today starting at $3,350.

Product number

Bandwidth

Channels

Price ($)

DSOX3012T

100 MHz

Two analog

3,350

DSOX3014T

100 MHz

Four analog

3,990

DSOX3022T

200 MHz

Two analog

3,990

DSOX3024T

200 MHz

Four analog

4,450

DSOX3032T

350 MHz

Two analog

6,900

DSOX3034T

350 MHz

Four analog

8,300

DSOX3052T

500 MHz

Two analog

8,750

DSOX3054T

500 MHz

Four analog

11,200

DSOX3102T

1 GHz

Two analog

10,500

DSOX3104T

1 GHz

Four analog

13,900

MSOX3012T

100 MHz

Two analog plus 16 digital

4,850

MSOX3014T

100 MHz

Four analog plus 16 digital

5,490

MSOX3022T

200 MHz

Two analog plus 16 digital

5,490

MSOX3024T

200 MHz

Four analog plus 16 digital

5,950

MSOX3032T

350 MHz

Two analog plus 16 digital

8,400

MSOX3034T

350 MHz

Four analog plus 16 digital

9,800

MSOX3052T

500 MHz

Two analog plus 16 digital

10,250

MSOX3054T

500 MHz

Four analog plus 16 digital

12,700

MSOX3102T

1 GHz

Two analog plus 16 digital

12,000

MSOX3104T

1 GHz

Four analog plus 16 digital

15,400

Information about the InfiniiVision 3000T X-Series oscilloscopes is available at www.keysight.com/find/3000TX-Series. Product images are available at http://www.keysight.com/find/3000TX-Series_images. A product video is available at www.keysight.com/find/3000TX-Series_video.

Information about the company's complete line of oscilloscopes is available at www.keysight.com/find/scopes.
About Keysight Technologies

Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com