Keysight Technologies Introduces Industry's First DisplayPort 1.3 Source Electrical Performance, Validation, Compliance Software

  
  

New Software Helps Engineers Accomplish Their DisplayPort Characterization Tasks with Confidence, Thoroughness

Highlights:

  • Builds on current standard DisplayPort certification solution
  • Designed to support future DisplayPort compliance test specification(s)
  • Supports DisplayPort over USB Type-C™ Designs

SANTA ROSA, Calif., Dec. 9, 2015

Keysight Technologies, Inc. (NYSE: KEYS) today announced the industry's first DisplayPort 1.3 source compliance and validation software. The U7232D DisplayPort 1.3 compliance and validation test software runs on Keysight's industry-leading Infiniium oscilloscopes and provides a complete compliance test suite for the extensive physical-layer tests required for DisplayPort 1.3 source devices.

The DisplayPort specification defines a digital audio/video interconnect used primarily between a computer and its monitor or a computer and a home-theater system. The Video Electronics Standard Association (VESA) released the DisplayPort 1.3 specification in September 2014 and is close to releasing the related compliance test specification. The DisplayPort 1.3 specification, and soon to be released, DisplayPort 1.4, increases the possible data rate to 8.1 Gbs and adds new measurement methods and patterns, further complicating the process of validating all possible DisplayPort states.

Transmitting data robustly at 8.1 Gbs over inexpensive media such as standard or flexible PC boards requires pre-emphasis constructs in the transmitter, and receivers must employ a minimum equalization to decode the data. The transmitter tests require that a mathematical worst-case channel model be used on the source before a reference equalizer is employed to make the source eye diagram and jitter measurements. The reference equalizer included for HBR3 (8.1 Gbs) includes a decision feedback equalizer much like that used in USB 3.1.

"Keysight's compliance test software solutions have been an ongoing, key aspect of the DisplayPort ecosystem and interoperability program, and VESA is pleased to see Keysight continue to make major contributions in phy layer testing as we move into DisplayPort 1.3 and beyond," said Bill Lempesis, executive director of VESA, the organization that oversees the DisplayPort specification.

Keysight's DisplayPort 1.3 source compliance and validation software makes these measurements automatically and builds on the usability and configurability of previous-generation compliance test software. As a result, engineers can continue to count on the usability and accuracy they have enjoyed in the past.

"DisplayPort technology demands a flexible, configurable tool that can be employed in a variety of use models – from characterization of transmitter integrated circuits to compliance testing of systems," said Dave Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "Our DisplayPort compliance test software gives engineers that flexibility and helps them confidently and thoroughly accomplish their DisplayPort characterization tasks."

Features of the U7232D DisplayPort 1.3 source compliance and validation software include:

  • Full physical-layer testing of the high-speed DisplayPort lanes
  • Support for multiple standards (DisplayPort 1.2a and DisplayPort 1.3)
  • Physical-layer AUX channel tests
  • Test automation support
  • Guided device and test setup system
  • Measurement parameter configurability for debugging

In addition to the U7232D software, Keysight DisplayPort test solutions include:

  • DSAV1604A or DSA 90000 X-Series Infiniium oscilloscopes
  • DisplayPort test-point adapter, such as the N7015A for the USB Type-C connector or other appropriate test-point adapter such as the BIT-mDP-PTF-0001 from Bitifeye Corp
  • Oscilloscope amplifiers and probes (optional)
  • Switch Matrix for sequenced testing of multiple lanes (optional)
  • Unigraf DPR-100 AUX channel controller (optional)

U.S. Pricing and Availability

  • 16-GHz Infiniium oscilloscopes start at $150,000
  • The new U7232D fully-featured (Option 1FP) is $8,000
  • The upgrade from DisplayPort 1.2 version (Option 2FP) is $4,000
  • The N7015A test-point adapter is $10,000

More information about the Keysight DisplayPort 1.3 source compliance and validation software is available at www.keysight.com/find/U7232D. Images are available at http://www.keysight.com/find/U7232d_images.

About Keysight in Software

Keysight software is downloadable design, test and measurement expertise. From first simulation through first customer shipment, Keysight software tools enable engineering teams to accelerate from data to information to actionable insight. Additional information is available at www.keysight.com/find/software Download free software trials at www.keysight.com/find/free_trials.

About Keysight Digital Test Solutions

Keysight's solutions for digital applications are driven and supported by Keysight experts who are involved in various international standards committees. Keysight experts are active in the Joint Electronic Devices Engineering Council (JEDEC), PCI Special Interest Group (PCI-SIG®), Video Electronics Standards Association (VESA), Serial ATA International Organization (SATA-IO), USB Implementers Forum (USB-IF), Mobile Industry Processor Interface (MIPI™) Alliance, Ethernet standards (IEEE 802.3), Optical Internetworking Forum (OIF) and many others. Keysight is committed to involvement in standards groups and related workshops, plugfests and seminars to ensure the right test solutions are created to meet customers' evolving needs.
About Keysight Technologies

Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.

# # #

USB Type-C™ and USB-C™ are trademarks of USB Implementers Forum.

PCI-SIG, PCI Express, PCIe and M-PCIe are trademarks or registered trademarks of PCI-SIG