SANTA ROSA, Calif., March 9, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today announced that its N7617B Signal Studio for 802.11 WLAN software is the industry's first flexible 802.11ah signal creation solution and supports a variety of Keysight vector signal generators. Signal Studio provides flexible, standard-based waveforms, perfect for testing 802.11ah-enabled Internet-of-Things (IoT) devices. With this announcement, Signal Studio now supports all major evolutions of the 802.11 standard, including 802.11a/b/g/j/p and 802.11n/ac.
IEEE 802.11ah is an emerging standard that defines a WLAN system operating in sub 1-GHz, license-exempt bands. This emerging standard is viewed as a key enabler of IoT devices, relying on power efficient, long range and scalable Wi-Fi services. Compared to existing 802.11 standards operating in the 2.4 GHz and 5 GHz bands, 802.11ah offers a significantly improved transmission range. This makes it ideal for use in large-scale sensor networks, extended range hotspots, power efficient devices, and outdoor Wi-Fi for cellular traffic offloading.
Keysight's Signal Studio for WLAN reduces the time spent on signal creation. Its application-specific interface supports all physical layer parameters enabling users to create and customize standards-based, performance-validated signals for component, transmitter and receiver test. Designers can use the basic capabilities (Option JFP) of the software to create partially-coded signals for transmitter or component test, while the advanced capabilities, Option UFP, creates fully-coded signals for receiver test.
After the creation of the 802.11ah-compliant reference signals, engineers can download them to a variety of Keysight instruments for real-world testing. The Signal Studio for WLAN software supports Keysight's bench-top vector signal generators (MXG, EXG, ESG, and PSG), the modular M9381A PXI vector signal generator and the E6640A EXM one-box tester. Such functionality is critical to helping WLAN industry chipset vendors, consumer electronics, wearable devices and home automation makers develop, validate and produce early products based on the 802.11ah standard.
"As a recognized industry leader in the wireless test industry, Keysight is actively involved in the development and implementation of emerging standards such as 802.11ah, and an enabler of emerging market segments like the Internet-of-Things," said Mike Griffin, applications marketing manager for Keysight's Microwave and Communications Division. "Keysight's new Signal Studio 802.11ah capability provides designers the benchmark solution they need to confidently move their 802.11ah-based designs forward, and in the process, will play a pivotal role in aiding the build-out of the Internet-of-Things."
U.S. Pricing and Availability
Keysight's N7617B Signal Studio for 802.11 WLAN is available now. Pricing is as follows:
N7617B-JFP | Basic 802.11ah WLAN | $2,800 |
N7617B-UFP | Advanced 802.11ah WLAN | $2,200 |
For more information about Keysight's 802.11 WLAN signal creation software, visit www.keysight.com/find/N7617B. An image of the software with support for the 802.11ah standard is available at www.keysight.com/find/N7617B_images.
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com