Highlights:
SANTA ROSA, Calif., Oct. 13, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced a logic analyzer module with the industry's highest-data-rate state mode (up to 4 Gb/s), highest timing mode (10 GHz) and deepest memory depth (up to 400 MB). Keysight also introduced two W4640A Series DDR4 BGA interposers with zero insertion force (ZIF) probe/cables, and Soft Touch Pro connectorless probe cables that enable engineers to validate and debug simultaneous read and write DDR4 or LPDDR4 traffic operating at data rates up to 4 Gb/s.
The Keysight U4164A logic analyzer is designed for engineers who work on high-end digital designs, mobile, computing, DDR/LPDDR memory and server applications. The U4164A combines its industry-leading state capture speed with the ability to reliably capture data on the industry's smallest eye openings (as small as 100 ps by 100 mV). These capabilities allow engineers to measure the increasingly fast digital signals used in emerging technologies and validate and troubleshoot their designs with confidence.
"DDR4 and LPDDR4 memory speeds continue to increase, probing space decreases and new power-saving modes of memory technologies are being enabled, making reliable measurements and analysis more critical," said Dave Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "Keysight's new technology in the U4164A logic analyzer, new probing products and software analysis tools help our customers continue to capture live high-speed traffic so they can understand, debug and validate their digital systems as bus speeds increase."
The U4164A logic analyzer module has two new modes of operation: quad-sample state mode and 10-GHz quarter-channel timing mode. In addition to the new modes of operation, the U4164A logic analyzer module includes new features to help high-speed digital and DDR/LPDDR memory design engineers turn on and debug their systems faster. New features include a timing mode deskew control, dual thresholds in dual-sample state mode, and clock hysteresis control to adjust the state mode sensitivity to noise on clock inputs.
The U4164A's new modes of operation enable new probing methods, including the U4206A Soft Touch Pro direct-connect probe/cable designed exclusively for use with the U4164A. New W4640A Series DDR4 two-wing BGA interposers (W4643A for DDR4 x4/x8 and W4641A for DDR4 x16 DRAM probing) take full advantage of quad-sample state mode on the U4164A and are the smallest BGA interposers for DDR4 capable of capturing simultaneous read and write traffic greater than 3.2 Gb/s. New U4208A and U4209A probe/cables connect the W4640A Series DDR4 BGA interposers directly into the U4164A logic analyzer module with 61-pin high-density zero insertion force (ZIF) connectors at the W4640A wings.
Engineers can merge up to three U4164A logic analysis modules to capture DDR4 DIMM traffic at data rates already proven up to 4 Gb/s using the FS2510AB DDR4 DIMM interposer from Keysight Strategic Solutions Partner FuturePlus Systems.
The exclusive eye-scan capability of the U4164A gives engineers a quick overview of signal integrity on all signals of a DDR system in a fraction of the time it takes using alternative methods.
Keysight's comprehensive DDR/LPDDR solution portfolio continues to expand across all stages of DDR chip development to help engineers overcome tough DDR and LPDDR troubleshooting and probing challenges.
The U4164A logic analyzer module is compatible with Keysight's M9502A two-slot and M9505A five-slot AXIe chassis. Multiple modular systems can be combined for time-correlated measurements on multiple buses in a system.
U.S. Pricing and Availability
The Keysight U4164A logic analyzer modules can be ordered today at a starting price of $33,366 for 136 channels, 350-MHz state clock, including chassis, but not including probes, cables or optional software. Shipments will begin in December.
Additional information
Additional information about Keysight's U4164A logic analyzer module is available at www.keysight.com/find/U4164A. Product images are available at http://www.keysight.com/find/U4164A_images.
Additional information about Keysight's W4641A DDR4 x16 and W4643A DDR4 x4/x8 2-wing 3.2-Gb/s BGA interposers with associated ZIF probe/cabling are available at www.keysight.com/find/W4641A and www.keysight.com/find/W4643A.
Additional information about Keysight's memory analysis software with performance and compliance test solutions for logic analysis is available at www.keysight.com/find/B4661A.
Keysight will feature the new Keysight U4164A at MemCon in Santa Clara, Calif. on October 13 and at DesignCon in Santa Clara, Calif. in January 2016.
Information about compatible probes, made by Keysight channel partner FuturePlus, is available at www.keysight.com/find/FuturePlus.
Keysight's Digital Test Standards Program
Keysight's solutions for digital applications are driven and supported by Keysight experts who are involved in various international standards committees. Keysight experts are active in the Joint Electronic Devices Engineering Council (JEDEC), PCI Special Interest Group (PCI-SIG®), Video Electronics Standards Association (VESA), Serial ATA International Organization (SATA-IO), USB Implementers Forum (USB-IF), Mobile Industry Processor Interface (MIPI™) Alliance, Ethernet standards (IEEE 802.3), Optical Internetworking Forum (OIF) and many others. Keysight is committed to involvement in standards groups and related workshops, plugfests and seminars to ensure the right test solutions are created to meet customers' evolving needs.
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com