Highlights:
SANTA ROSA, Calif., Oct. 14, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced an enhanced signal processing configuration for its M9703B 12-bit AXIe high-speed digitizer/wideband digital receiver. System architects and engineers can use this new bundle option, which is ideal for OEM and aerospace & defense applications, as a component of a larger system requiring extensive FPGA capabilities and a high number of customizable real-time IO interfaces.
The M9703B-B01 bundle comes pre-configured with the following available options:
The U5340A FPGA Development Kit, a standalone software package, allows system architects and engineers to implement their own complex algorithm on-board the M9703B high-speed digitizer as well as to address the I/O to monitor and control their OEM system.
"Thanks to an unprecedented combination of 192 digital I/Os, eight high-speed, 12-bit analog input channels and a scalable open FPGA architecture, the new M9703B-B01 product provides the most versatile and customizable AXIe digitizer platform solution in a compact 1U form factor," said Pierre-François Maistre, Keysight Communication Measurement Solutions R&D project manager. "By providing wideband solutions that support advanced signal capture, Keysight aims to address more complex challenges in a large variety of aerospace & defense applications that require the treatment of a high amount of data and the control of very large systems."
Price and Availability
The new B01 bundle option is available now for the M9703B AXIe 12-bit high-speed digitizer/wideband digital receiver. Please contact [email protected] for more information.
Information about product configuration is available at www.keysight.com/find/M9703B.
High-resolution images are available at www.keysight.com/find/enhanced_signal_processing_axie_digitizers_images.
About Keysight High-Speed Digitizers
Keysight high-speed digitizers are the result of more than 300 years of cumulative research and development experience in analog-to-digital conversion technology. This ensures the ability to achieve the most effective and reliable analog-to-digital conversion at high-resolution and fast sampling rates. Information on the technology and its applications is available at www.keysight.com/find/high‑speed‑digitizers.
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]