SANTA ROSA, Calif., Feb. 17, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced a new ball grid array (BGA) interposer solution for testing DDR4 x16 DRAM designs with a logic analyzer. The interposer solution provides fast, accurate capture of address, command and data signals for debugging designs and making validation measurements. The Keysight W4631A BGA interposer, the world's fastest interposer solution for use with a logic analyzer, is used with Keysight's E5849A probes for high-data-rate DDR4 DRAM designs.
As the industry transitions to DDR4 data rates up to 3.2 Gb/s, engineers working on next-generation memory systems – such as those used in servers and embedded devices – face significant challenges. Probing and accurate signal capture are becoming increasingly critical for debug and validation of new designs.
The W4631A interposer solution solves probing connectivity by providing access to DDR4 x16 DRAM signals critical to debug and validation efforts. The probe works in many existing designs and eliminates the need for up-front planning or redesign. The probe connects directly to the balls of the DRAM with a DDR4 96 ball riser (included) or an optional 3rd party socket (not provided), enabling operation and acquisition of high-speed DDR4 signals with low loading and minimal impact to signal integrity on embedded system design. The interposer solution is designed to be used with the U4154B logic analyzer system.
The Keysight W4631A BGA interposer is designed for data rates up to 3.2 Gb/s. The probes are used with the U4154B logic analyzer to perform functional tests.
"Our customers need more accurate tools to achieve 3.2 Gb/s data rates and implement power-saving functionality," said David Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "With the new interposer, probes and logic analyzer system, engineers are ready to test DDR4 x16 data rates beyond today's data rates of 2400 Mb/s."
Features of the Keysight DDR x16 test solutions include:
Additional information about Keysight's W4631A BGA interposer is available at www.keysight.com/find/W4631A. Additional information about Keysight's U4154B logic analyzer family is available at www.keysight.com/find/U4154B. Product images are available at www.keysight.com/find/BGAinterposers_images. Additional information about Keysight's high-speed digital technologies is available at www.keysight.com/find/hsd. Additional information about Keysight's family of logic analyzers is available at www.keysight.com/find/LogicAnalyzer.
U.S. Pricing and Availability
The Keysight DDR4 x16 DRAM probing capability can be ordered now, with prices starting at $10,316.
The complete U4154B logic analyzer system for probing DDR4 x16 DRAM start at $97,673.
Keysight's Digital Test Standards Program
Keysight's solutions for digital applications are driven and supported by Keysight experts who are involved in various international standards committees. Keysight experts are active in the Joint Electronic Devices Engineering Council (JEDEC), PCI Special Interest Group (PCI-SIG®), Video Electronics Standards Association (VESA), Serial ATA International Organization (SATA-IO), USB Implementers Forum (USB-IF), Mobile Industry Processor Interface (MIPI™) Alliance, Ethernet standards (IEEE 802.3), Optical Internetworking Forum (OIF) and many others. Keysight is committed to involvement in standards groups and their related workshops, plugfests and seminars to ensure the right test solutions are created to meet customers' evolving needsKeysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
PCI-SIG® is a US registered trademark and/or service mark of PCI-SIG.
MIPI is a licensed trademark of MIPI, Inc. in the U.S. and other jurisdictions.
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com