Here’s the page we think you wanted. See search results instead:

 

Keysight Technologies Adds Versatile Performance Options to Industry's Fastest Power Supplies

  
  

New Options Allow Engineers to Tune Power Supplies for Optimum Balance of Test Coverage, Quality, Time

SANTA ROSA, Calif., April 23, 2015

Keysight Technologies, Inc. (NYSE: KEYS) today introduced four performance options for its small, flexible and market-leading-fast Advanced Power System (APS) N6900 Series DC power supplies. In conjunction with the power supply's VersaPower architecture, the new options boost test-system versatility and make it easy for test engineers to tune power supply capability. The N6900 options enable engineers to meet their ATE testing needs without paying for more capability than they require.

The new options include:

  • An accuracy package (Option 301), which adds a second seamless measurement range for current, with full factory calibration
  • Measurement enhancements (Option 302), which add external data logging and voltage and current digitizers with programmable sample rates
  • Source and speed enhancements (Option 303), which add constant-dwell arbitrary waveforms and output list capability and provide improvement in up/down programming time
  • Disconnect and polarity-reversal relays (Options 760 and 761), which allows engineers to switch voltages between positive and negative values

Using the new options, engineers can integrate and deploy their test systems faster while achieving test speeds that are up to 100 times faster than is possible with standard system power supplies. The faster throughput speeds can help manufacturers reduce test costs. The smaller size of the APS N6900 power supplies saves rack space, which also can reduce test costs.

Using the APS N6900 power supplies, engineers can accurately characterize DUT power profiles with advanced measurement capabilities. For example, engineers can:

  • Perform dual voltage and current measurements with DMM-like accuracy
  • Make dynamic measurements with high-resolution digitizers for current and voltage (with measurement option)
  • Easily measure power, peak power, watt hours and amp hours

The core design of the APS power supply family is built on Keysight's VersaPower architecture, which uses cutting-edge technology to deliver industry-leading performance and adds innovative capabilities previously unavailable in switching power supply designs. The APS family includes the Keysight N6900, N7900 and N6700 Series DC power supplies.

The Keysight APS N6900 Series DC power supplies include five voltage and current combinations at the 1-kW power range and seven voltage and current combinations at the 2-kW power range. The 1-kW models are 1U tall and the 2-kW models are 2U tall.

Additional information about the new options for Keysight's APS N6900 Series DC power supplies is available at www.keysight.com/find/N6900options. Product images are available at www.keysight.com/find/N6900options_images .

Through December 31, Keysight is offering a promotion on APS N6900 DC power supplies that allows engineers to save up to 20 percent off the purchase price. More information is available at www.keysight.com/find/N6900Promo.

U.S. Pricing and Availability

Keysight APS N6900 power supplies with options installed are orderable now. The starting price for 1-kW models is $5,711; the starting price for 2-kW models is $7,715.
About Keysight Technologies

Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com