SANTA ROSA, Calif., March 24, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced measurement software designed to help engineers quickly and accurately characterize PAM-4 (pulse amplitude modulation with four amplitude levels) signals using the Keysight V-Series, Z-Series, and S-Series real-time oscilloscope platforms. The Keysight N8827A PAM-4 analysis software (for V- and Z-Series oscilloscopes) and N8827B PAM-4 analysis software (for S-Series oscilloscopes) provides comprehensive analysis of electrical PAM-4 signals.
Mobile computing applications are demanding more of the underlying computer Internet infrastructure. To enable increases in Internet and server-farm performance, higher-speed connectivity among server systems is required. Conventional communication techniques often relied upon NRZ (non-return-to-zero) encoding. Industry experts contend NRZ will not work in a 56-GBit/s environment. One way to overcome this challenge is to change the modulation technique from NRZ to pulse amplitude modulation. This allows engineers to dramatically increase the amount of data they can send across high-speed digital communication links.
Several industry standards bodies are actively promoting PAM-4 technology to enable the next-generation speed class and push higher data rates for a given channel compared to traditional NRZ signaling. While PAM-4 technology leverages some traditional NRZ measurement algorithms for PAM-4 signals, to fully analyze system performance, unique PAM-4 measurements and parameters are required.
"Our customers face many new design and measurement challenges as they make the switch from NRZ to PAM-4 signaling," said Dave Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "By delivering both analysis and debug capabilities for PAM-4 signals, our latest PAM-4 analysis software for our real-time oscilloscopes helps engineers address these challenges and quickly get their designs to market."
N8827A/B PAM-4 analysis software offers measurements such as:
Engineers can combine the N8827A/B PAM-4 option with existing Infiniium real-time oscilloscope software tools to provide even more powerful analysis capability:
Multilevel signaling systems are particularly susceptible to noise, so the V-Series, Z-Series and S-Series real time oscilloscopes offer the industry's lowest noise floors for wide bandwidth real-time oscilloscopes. When using the 63 GHz Z-Series oscilloscope, for example, designers can achieve accurate analysis of electrical PAM-4 signals to 32 Gbaud. Additionally, engineers can perform offline analysis on stored PAM-4 signals using the N8900A Infiniium Offline oscilloscope analysis software installed on a PC.
Additional information about Keysight's PAM-4 analysis software is available at www.keysight.com/find/N8827A and www.keysight.com/find/N8827B. Product images are available at www.keysight.com/find/PAM4scopes_images.
Keysight will demonstrate high-speed digital test solutions, including PAM-4 generation and measurement capability, at OFC 2015, Booth 1201, at the Los Angeles Convention Center, March 24-26.
Visit Keysight's PAM-4 oscilloscope solutions website for more information about all scope PAM-4 solutions.
U.S. Pricing and Availability
N8827A and N8872B software applications will be orderable on April 7. Each application is priced at $7,500.
Keysight's Digital Test Standards Program
Keysight's solutions for digital applications are driven and supported by Keysight experts who are involved in various international standards committees. Keysight experts are active in the Joint Electronic Devices Engineering Council (JEDEC), PCI Special Interest Group (PCI-SIG®), Video Electronics Standards Association (VESA), Serial ATA International Organization (SATA-IO), USB Implementers Forum (USB-IF), Mobile Industry Processor Interface (MIPI™) Alliance, Ethernet standards (IEEE 802.3), Optical Internetworking Forum (OIF) and many others. Keysight is committed to involvement in standards groups and related workshops, plugfests and seminars to ensure the right test solutions are created to meet customers' evolving needs.Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com