SANTA ROSA, Calif., Feb. 26, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced the bandwidth enhanced N7000A InfiniiMax III+ differential probes for general-purpose, high-speed differential bus probing. The company also introduced an active termination adapter that provides ultra-low noise voltage termination to a non-ground signal, and QuickTip accessories for InfiniiMax I/II probes to help engineers make quick and reliable measurements.
The InfiniiMax III+ probes work with the full array of InfiniiMax III probe heads, including a wide range of solder-in probe heads, a browser head, ZIF (zero insertion force) tips, 2.92-mm/3.5-mm/SMA heads and the QuickTip head. These probing solutions complement the new Infiniium V-Series oscilloscopes with its revolutionary industry-leading performance, accuracy and ease of use.
Keysight’s InfiniiMax III+ probes offer InfiniiMode technology, which greatly expands the measurement capabilities and usability of the probe, making it capable of measuring all the components of a differential signal. With a single connection, engineers can set the InfiniiMax III+ to measure the differential signal, the single-ended A or B signals, and the common-mode component of a differential signal.
As with InfiniiMax III technology, the unique S-parameters of each InfiniiMax III+ probe amp are stored in the probe amp and are used with the S-parameters of the various probe heads. This further flattens the magnitude and phase response of the probe for higher accuracy.
To date, most oscilloscopes with 50 ohm inputs terminate to ground. However, some communication system standards, such as HDMI 2.0, DisplayPort and MIPI M-PHY Gear 3/4, require the 50 ohm termination to a voltage rather than to ground. The Keysight N7010A active termination adapter is a 30 GHz single-ended adapter featuring a user-adjustable common termination voltage (VTERM) and extremely low noise performance. The oscilloscope can internally control the termination voltage to keep it between -4.0 V to +4.0 V. Utilizing low attenuation ratio setting (1.16:1), the adapter enables extremely lower noise floor.
For high-speed signal probing, solder-in probe heads are commonly used. Unfortunately, solder-in probes are not the ideal solution when it comes to moving around multiple test points on a target board. The N2851A QuickTip probe head for InfiniiMax I/II provides the industry’s only quick connect/disconnect capability when measuring multiple high-speed test points. The QuickTip design uses three small, gold-plated magnets as the actual contacts to gold-plated steel buttons on the probe tip. Engineers can install multiple N2849A probe tips on a device under test, allowing quick and reliable measurements of many probe points.
“Keysight believes we must innovate on multiple fronts to provide insight for our customers,” said Dave Cipriani, vice president and general manager of Keysight’s Oscilloscope and Protocol Division. “Simply moving ahead on a banner spec doesn’t help them. That is why today, Keysight is introducing a family of oscilloscopes and probing solutions that deliver new capability while improving ease of use.”
Additional information about Keysight’s new InfiniiMax III+ probing system and QuickTip accessories is available at www.keysight.com/find/InfiniiMax. Product images are available at www.keysight.com/find/InfiniiMax_images.
U.S. Pricing and Availability
Keysight InfiniiMax III+ and accessory products can be ordered today at the prices listed below. Limited shipments will begin in April.
Model Description Price N7000A InfiniiMax III+ 8-GHz probe amplifier $8,000 N7001A InfiniiMax III+ 13-GHz probe amplifier $12,000 N7002A InfiniiMax III+ 16-GHz probe amplifier $17,000 N7003A InfiniiMax III+ 20-GHz probe amplifier $20,000 N7010A 30-GHz Active Termination Adapter $5,000 N2851A QuickTip probe head for InfiniiMax I/II $1,000
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com