SANTA ROSA, Calif., July 27, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today announced the addition of two higher temperature models to its thermal imagers' portfolio. The U5856A and U5857A can perform temperature measurements up to 650 degrees C and 1200 degrees C respectively. This allows users to detect a wide temperature range for various applications such as petrochemical and steel processing, electrical and mechanical applications, building maintenance and even electronics applications.
With the shift towards predictive maintenance in industrial settings, the U5850 series allows technicians and engineers to efficiently and safely detect abnormalities without shutting down the system. Keysight's U5850 series TrueIR thermal imagers is among the first in its range of thermal imagers that include four times in-camera fine resolution of 320 x 240 pixels from a 160 x 120 pixel detector. Together with the manual focus feature, allowing users to focus on an object as close as 10 cm, our solution provides clearer, sharper and reveals finer details to detect problems even faster.
The U5850 series offers image logging and temperature trending capabilities to monitor temperature changes overtime for accurate quality checks and diagnostic purposes. With a good 0.07 degree C thermal sensitivity, users can capture, save and analyze temperature changes accurately. For more in-depth analysis and report generation, technicians and engineers can use the TrueIR Analysis and Reporting Tool PC software, which they can download for free at www.keysight.com/find/TrueIR_ART.
"Our customers can have the utmost confidence in our expanded portfolio of thermal imagers with the improved overall usability," said Ee Huei Sin, vice president, Keysight's General-Purpose Electronic Measurement Division. "Our ongoing goal is to offer dependable tools that provide a wealth of essential and innovative capabilities, while retaining ease of use."
The award winning U5855A's compact, light and ergonomic design allows engineers to comfortably use the thermal imager for longer periods of time, and operate it single-handedly in tight locations. Users can also easily change settings or access frequently used functions such as flash light, laser pointer, auto scaling or simply capture thermal image with quick access buttons. With the easy-to-use customizable color palette, users can now customize the right color palettes for their applications.
Additional information about Keysight's U5850 series TrueIR thermal imagers is available at www.keysight.com/find/trueIRimagerSeries_pr.
Product images are available at www.keysight.com/find/trueIRimagerSeries_images.
A product video is available at www.keysight.com/find/trueIRimagerSeries_video.
A complete list of handheld tools videos is available at on YouTube.
U.S. Pricing and Availability
The new U5850 series TrueIR thermal imagers are available worldwide, at the following prices:
Product |
Model |
Description |
Price |
Thermal Imager |
U5855A |
TrueIR thermal imager, up to 350 °C |
$3,507 |
Thermal Imager |
U5856A |
TrueIR thermal imager, up to 650 °C |
$3,995 |
Thermal Imager |
U5857A |
TrueIR thermal imager, up to 1200 °C |
$5,495 |
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com