SANTA ROSA, Calif., Jan. 28, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced N1930B Physical Layer Test System (PLTS) 2015, the latest release of its premier signal integrity test software for designing and validating high-speed digital interconnect.
A key software enhancement in PLTS 2015 includes an N-port automatic fixture removal (AFR). This enhancement removes the effects of multiple test fixtures with a single step – reducing the error-correction time by 75 percent when compared to other traditional error correction methods.
The N-port AFR de-embedding process measures the open circuit of multiple fixtures. This allows engineers to easily remove the unwanted effects of these fixtures in just a single pass of the AFR process. Specifically, the traditional Through-Reflect-Line calibration process has over 150 steps of calibration, while the N-port AFR has less than 10 error correction steps. Additionally, the N-port AFR technique eliminates design and fabrication costs for special calibration boards.
Additional PLTS 2015 Enhancements
PLTS now provides support for Keysight's award winning modular PXI vector network analyzers (VNAs). Leveraging the multiple ports (up to 32) of the PXI VNAs, engineers can now characterize eight differential channels in one measurement. Additionally, the graphical user interface easily manages over 900 S-parameters in one data file. When multiple data channels are analyzed at once, additional insight is gained into the device characteristics and data management is simplified.
Another powerful new feature found in PLTS 2015 is the round robin wizard. This wizard makes it possible for engineers to measure a device under test with more ports than the VNA they use in their lab. For example, they can use a 4-port VNA to measure a 12-port device. PLTS provides step-by-step instructions and then outputs a 12-port data file in various formats. The data is saved in one file, just as if the measurement had been made with a 12-port VNA. This ability to analyze large port-count data files provides users tremendous insight into critical performance parameters such as near-end and far-end crosstalk.
U.S. Pricing and Availability
Keysight's N1930B PLTS 2015 is available now at a base price of $10,000. Keysight will demonstrate the software for the first time at DesignCon 2015, Booth 725, Santa Clara Convention Center, Jan. 28-29.
More information about the PLTS 2015 software is available at www.keysight.com/find/plts. A video demonstration detailing how engineers can measure 32 interconnect devices using a PXI VNA with PLTS software for multi-port multi-domain device characterization is available on YouTube. An image of the software is available at www.keysight.com/find/PLTS2015_images.Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]