SANTA ROSA, Calif., Jan. 29, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced the first power analyzer that combines accurate power measurements and touch-driven oscilloscope visualization capability in a single instrument. The Keysight IntegraVision power analyzer makes it easy for R&D engineers who are designing and testing electronic power conversion systems to access dynamic views of current, voltage and power so they can see, measure and prove the performance of their designs.
Engineers working on electronic power conversion systems need high-accuracy measurements to identify and characterize incremental efficiency improvements in devices such as power inverters or converters, universal power supplies, battery systems, vehicle and aircraft power systems, lighting systems/electronic ballasts and appliances. While some of today's power analyzers offer adequate measurement accuracy, they are cumbersome to use and lack the ability to characterize power consumption under dynamic conditions. Previously, engineers needed a power analyzer to make accurate measurements and an oscilloscope to visualize repetitive and single-shot events such as turn-on and occurrences of transients. Eliminating a separate oscilloscope in the measurement setup decreases test complexity and reduces configuration time.
The Keysight IntegraVision power analyzers are ideal for R&D engineers who want to quickly and interactively measure AC and DC power consumption, power conversion efficiency, operational response to stimulus and common AC power parameters such as frequency, phase and harmonics – all with 0.05 percent basic accuracy and 16-bit resolution. The power analyzer enables engineers to characterize power consumption under highly dynamic conditions with 5-M samples per second digitizing speed and 2-MHz bandwidth.
"With power analyzer accuracy and scope-like waveform visualization in a single instrument, IntegraVision power analyzers make it significantly easier for R&D and design validation engineers to pinpoint and fix problems or optimize the power efficiency of their designs," said Kari Fauber, general manager of Keysight's Power and Energy Division. "If engineers can use an oscilloscope, they already know how to use this instrument, so the learning curve is minimal. With the touch screen, power measurements are no longer time consuming and tedious."
The IntegraVision power analyzer allows engineers to address multiple test scenarios with the flexibility of wide-ranging, isolated inputs up to 1,000 Vrms (Cat II). The instruments offer external sensor inputs and 2-Arms and 50-Arms direct current inputs, standard on all channels. The external sensor input supports current probes and transducers up to 10-V full scale.
The IntegraVision power analyzer features a space-efficient footprint and allows engineers to:
The user interface of the IntegraVision power analyzers is based on technology from Keysight's InfiniiVision 6000 X-Series oscilloscope, including its 12.1-inch multitouch capacitive touchscreen with pinch, zoom and scroll capabilities. Keysight's development of the user interface was guided by extensive feedback from engineers. The result is an intuitive user experience that enables engineers to gain measurement insight with the IntegraVision power analyzer within minutes.
Additional information about Keysight IntegraVision power analyzers is available at www.keysight.com/find/IntegraVision. Product images are available at www.keysight.com/find/IntegraVision_images. A video is available at www.keysight.com/find/PA2201A_video or on YouTube.
A backgrounder, "Understanding the Challenges of Power and Energy Measurements," is available at www.keysight.com/find/IntegraVision_backgrounder.
U.S. Pricing and Availability
The two-channel Keysight IntegraVision PA2201A power analyzer is suitable for single-phase AC measurements and can be ordered today. Shipments are expected to begin in May. Pricing is available upon request. The IntegraVision PA2203A power analyzer with four channels for three-phase power analysis is scheduled to be introduced in the fourth quarter of 2015.Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]