Keysight Technologies to Demonstrate Advance Communication Test and Measurement Solutions at ECOC 2016

  
  

400Gb/s Solutions Include Generation and Analyses of Coherent Optical Modulated Signals Required for Next-Generation Networking

Highlights:

  • Keysight will show new modulations techniques, such as PAM-4, that simplify accurate receiver testing for 400GbE devices
  • Keysight will show new and enhanced solutions for creating better designs, making validation easier, and speeding up manufacture test of components and systems

SANTA ROSA, Calif., Sept. 1, 2016

Keysight Technologies, Inc. (NYSE: KEYS) today announced that it will demonstrate test and measurement solutions designed to advance communications beyond 400Gb/s — from components through data center to telecommunications — at ECOC 2016, Stand 400, Düsseldorf, Germany, Sept. 19-21.

Demonstrations will include a variety of measurement solutions used in the characterization of electrical and optical transceivers and in component test.

  • New M8040A high-performance 64 GBaud BERT for PAM-4 and NRZ simplifies accurate receiver testing for 400GbE devices. This extension of the M8000 series of BER test solutions streamlines receiver test setups with its highly integrated pattern generator and ensures repeatable results with true PAM-4 error detection.
  • New N1092D DCA-M sampling oscilloscope for optical signals in a reduced cost platform operated with an external PC running the FLEX-DCA interface. The oscilloscope performs basic waveform analysis and industry compliance test for 25 G class optical transmitters. The sampling oscilloscope features low noise/high sensitivity (5 uW/ 4 dB better SNR), high throughput and low jitter (<200 fS). The new DCA-M sampling oscilloscope for optical transmitters will be the backbone for testing 25/50/100/200 and 400 Gb/s optical interconnects.
  • New N4917B optical receiver stress test solution for 100GBASE-LR4 transceivers represents the next generation of test automation. The N4917B provides accurate and repeatable receiver characterization for R&D and validation engineers so they can effectively evaluate their latest 100Gb Ethernet designs. The solution is based on the J-BERT M8020A high-performance BERT, including the M8062A 32Gb/s BERT front end, the 86100D Infiniium DCA-X high-bandwidth oscilloscope, 81490A reference transmitter and N77 series attenuator. The newly configured solution allows customers to use the build-in error counters or the BERTs integrated error detector.
  • Keysight EEsof EDA Advanced Design System, the world's leading electronic design automation software for RF, microwave and high-speed digital applications, features enhanced design and signal generation software solutions.
  • Keysight will demonstrate how engineers can use its end-to-end reference solution based on the 92GSa/s arbitrary waveform generator and modulation analyzer (N4391A) for the generation and analysis of optically impaired complex, multi-level and multichannel signals.
  • Keysight will also demonstrate the latest additions to its range of tunable laser sources and two-way swept-wavelength test solutions.
  • In addition, Keysight will demonstrate the only Indium Phosphide 63 GHz oscilloscope and show the latest software enhancements and expansion of its family of accessories in combination with the M8195A 65 GSa/s arbitrary waveform generator.

Keysight proudly supports ECOC 2016 and its Poster presentations. Thomas Dippon of Keysight is one of the coauthors of the Poster presentation "PAM-n Solutions for Low-Cost Implementations of 100 Gbps/Lambda Transmissions." Refer to the ECOC 2016 show program for additional information regarding times and locations.

Additional information about ECOC 2016 (www.ecocexhibition.com) and Keysight's products and services is available at www.keysight.com/find/ECOC2016.


About Keysight Technologies

Keysight Technologies (NYSE: KEYS) helps customers bring breakthrough electronic products and systems to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in the network. Customers span the worldwide communications ecosystem, internet infrastructure, aerospace & defense, automotive, semiconductor, and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2015. More information is available at www.keysight.com.