Keysight Technologies, Virginia Diodes, Inc. Selected by Chalmers University of Technology to Create World's First System for Network, Spectrum Analysis up to 1.5 THz

  
  

Measurement Capabilities Enable Deeper Insights as Chalmers Pursues Research into New Materials, Devices and Circuits

Highlights:

  • Unique capabilities enhance free-space, on-wafer and waveguide measurements of materials, devices and circuits at terahertz frequencies
  • Solution uses Keysight's PNA-X microwave network analyzer (10 MHz to 67 GHz) with integrated spectrum analysis capabilities
  • External extension modules from Virginia Diodes, Inc. (VDI) provide frequency coverage from 50 GHz to 1.5 THz

SANTA ROSA, Calif., Oct. 4, 2016

Keysight Technologies, Inc. (NYSE: KEYS) today announced that it has collaborated with Virginia Diodes, Inc. (VDI) to create a 1.5 THz measurement solution for Chalmers University of Technology, a leading research university located in Gothenburg, Sweden. Already up and running in Chalmers' national laboratory for terahertz characterization, this industry-first solution provides network and spectrum analysis capabilities for research on new materials, devices, and circuits for applications at micro-, millimeter- and sub-millimeter-wave frequencies.

Chalmers' researchers are working in the terahertz gap between radio waves and infrared light. The measurement equipment from Keysight Technologies provides new capabilities that are enhancing their work with free-space, on-wafer and waveguide measurements in the terahertz gap.

The system is built around the Keysight PNA-X microwave network analyzer, which covers 10 MHz to 67 GHz and reaches 1.5 THz with external extension modules from VDI. Achieving insightful understanding of device performance and behavior requires network and spectrum measurements, and the PNA family is the first to provide integrated spectrum analysis capability that reaches into the terahertz range. The ability to access both capabilities in a single test setup—and make multiple measurements through one set of connections—saves time and enhances insight.

"Working in concert with VDI, we're proud to be Chalmers' solution provider of choice for terahertz network and spectrum measurements," said Gregg Peters, vice president of Keysight's Aerospace & Defense Solutions Group. "As we keep reaching higher in frequency, our history of innovation will continue to enable new breakthroughs in science and technology."

"We are pleased to provide this premier research institution with extension modules that enable world-class science and engineering," added Tom Crowe, president and CEO of VDI. "It's another example of our ongoing work to open the terahertz spectrum for commercial and scientific applications."

Additional information is available at www.keysight.com/find/1.5THZ.

About Chalmers University of Technology

Chalmers University of Technology conducts research and offers education in technology, science, shipping and architecture in pursuit of its global vision for a sustainable future. Chalmers is well known for providing an effective environment for innovation and has eight priority areas of international significance: Building futures; energy; information and communication technology; life science engineering; materials science; nanoscience and nanotechnology; production; and transport. Additional information is available at www.chalmers.se/en.

About Virginia Diodes, Inc.

VDI's mission is to make the terahertz region of the electromagnetic spectrum as useful for scientific, military and commercial applications as the microwave and infrared bands are today. VDI manufactures state-of-the-art test and measurement equipment for millimeter-wave and terahertz applications. These products include extension modules that take the capabilities of high-performance microwave measurement tools—vector network analyzers, spectrum analyzers, and signal generators—to higher frequencies. More information is available at www.vadiodes.com.


About Keysight Technologies

Keysight Technologies (NYSE: KEYS) helps customers bring breakthrough electronic products and systems to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in the network. Customers span the worldwide communications ecosystem, internet infrastructure, aerospace & defense, automotive, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2015. More information is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]