Keysight Technologies Announces Low-Frequency Network Analyzer Options for Passive Component Characterization

  
  

Low-Frequency Options Offered at an Affordable Price

Highlights:

  • E5061B LF-RF network analyzer now effectively addresses the needs of a broad range of applications
  • An impedance analysis function for the low-frequency options enables customization in a single instrument

SANTA ROSA, Calif., April 6, 2016

Keysight Technologies, Inc. (NYSE: KEYS) today introduced a series of low-cost, low-frequency options for the E5061B LF-RF network analyzer.

Keysight's new low-frequency options expand the E5061B LF-RF network analyzer's ability to characterize passive components, including wireless power transfer and wireless charging systems, to a broad range of applications operating over a wider frequency range, from 5 Hz to 500 MHz (E5061B-3L3), 1.5 GHz (E5061B-3L4) and 3 GHz (E5061B-3L5).

"Our customers work in diverse fields with a diverse range of test needs and acceptable price points," said Akira Nukiyama, vice president and general manager of Keysight's Component Test Division, Kobe. "With our new low-frequency options for the ENA Series LF-RF network analyzer, we have given our customers the ability to cost-effectively test components at low frequencies, while still providing them a full and flexible frequency upgrade path from the low to high frequency."

Evaluating impedance characteristics of various electronic components is crucial to ensuring the performance and reliability of electronic equipment. With the E5061B-005 option, the E5061B LF-RF network analyzer combines network analysis and impedance analysis functions in a single instrument. The E5061B-005 option works with all E5061B LF-RF network analyzer frequency options.

More information on the E5061B LF-RF network analyzer options is available at www.keysight.com/find/ena-lf.

U.S. Pricing and Availability

Keysight's new low-cost, low-frequency options for the E5061B LF-RF network analyzer are available now. Pricing in U.S. dollars is as follows:

E5061B-3L3 E5061B network analyzer with LF-RF NA option
5 Hz – 500 MHz
$25,000
E5061B-3L4 E5061B network analyzer with LF-RF NA option
5 Hz – 1.5 GHz
$30,000
E5061B-3L5 E5061B network analyzer with LF-RF NA option
5 Hz – 3.0 GHz
$34,600
E5061BU-343 Upgrade option, from 500 MHz to 1.5 GHz $5,500
E5061BU-353 Upgrade option, from 500 MHz to 3.0 GHz $10,500
E5061BU-354 Upgrade option, from 1.5 GHz to 3.0 GHz $5,000

.


About Keysight Technologies

Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]