Highlights:
- LTE-A Pro end-to-end IP data throughput at 1Gbps and higher
- WLAN calling and offload, end-to-end VoLTE and integrated IMS
- Two-phone parallel RF test with 2G/3G/4G in a single test set
SANTA ROSA, Calif., Feb. 10, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today announced it will demonstrate the latest features of the E7515A UXM wireless test set at Mobile World Congress, Hall 2, Stand 2M2, Fira Gran Via, Barcelona, Feb. 22-25.
The demonstration will feature LTE-A Pro end-to-end IP data throughput of 1Gbps using three component carriers, 4x4 and 2x2 downlink MIMO, and 256QAM downlink modulation. Also on display is the UXM's first-to-market benchtop support for five component carrier (5CC) data throughput and 1.6Gbps data rates via 4CC carrier aggregation and 4x4 downlink MIMO.
Along with increased data throughput rates, the UXM further enhances device performance verification with support for 8x2 and 8x4 downlink MIMO, up to four component carriers in a single test set (in two bands), and an integrated iPerf network throughput tool.
"With support for download speeds beyond 1Gbps, the UXM's powerful platform continues to provide market-leading data throughput test capabilities," said Satish Dhanasekaran, general manager of Keysight's Wireless Devices and Operator Segment. "The latest UXM release also allows wireless device engineers to verify designs more efficiently with parallel test, VoLTE enhancements, and WLAN calling and offload."
Design engineers working to ensure seamless coverage with high-quality voice and data services will find the UXM's new enhanced VoLTE, WLAN calling/offload, dual-SIM test, and GSM/TD-SCDMA mobility features enable greater design confidence, on their benchtop. The UXM now supports UE-to-UE VoLTE calls in a single test set, as well as integrated IMS server capabilities such as IMS logging and easier configuration of dedicated bearers. Also available is WLAN calling and offload, to ensure WLAN-capable devices are able to transition smoothly between LTE-A and WLAN. The addition of GSM/GPRS/EGPRS and TD-SCDMA/HSPA test applications allow one-box interRAT testing between LTE and 2G/3G, including PS handovers, CSFB, and SRVCC.
The UXM's RF bench capabilities have also been expanded to reduce test time and cost of test with two-phone parallel RF test in a single UXM, one-box multi-format support including LTE/LTE-A, W-CDMA/HSPA+, TD-SCDMA/HSPA, and GSM/GPRS/EGPRS, as well as built-in CW interferers and the ability to change more connection parameters on the fly.
The UXM's receiver test capabilities including flexible channel definition, frequency division duplex (FDD) and time division duplex (TDD) options, along with out-of-channel measurements and integrated fading enable extensive coverage of 3GPP test cases in a conformance benchtop solution.
To schedule a demonstration of the UXM's latest enhancements at Mobile World Congress contact Keysight.
More information about Keysight's UXM wireless test set is available at www.keysight.com/find/UXM_enhancements. High resolution images are available at www.keysight.com/find/UXM_images. Videos demonstrating the UXM's versatile capabilities are available on YouTube. Contact Keysight at www.keysight.com/find/contactus for E7515A UXM pricing and delivery information.
About Keysight in Wireless
From WLAN to LTE-Advanced to the new 5G technologies, Keysight is focused on tackling the toughest design and test problems in the industry with the broadest range of solutions. With the most advanced electronic measurement solutions consisting of powerful software tied to both benchtop and modular hardware, engineers are able to get greater insight into design and test from simulation to R&D, from validation to manufacturing, from conformance to deployment. With experienced engineers in significant roles in cellular and WLAN standards groups and hundreds of application engineers all over the world, Keysight expertise is there to solve customer problems. Additional information is available at www.keysight.com/find/UXM and www.keysight.com/find/cellular. A knowledge library of application notes, CDs and more is available at www.keysight.com/find/cellular-insight.
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com