Highlights:
- Advanced low-frequency noise analyzer's integration with WaferPro Express enables turnkey noise measurements as well as measurement of DC characteristics, capacitance and RF S-parameters
- Software module measures DC characteristics, 1/f noise, random telegraph noise and conducts data analysis
- Keysight's close collaboration with Cascade Microtech enables a complete integrated on-wafer solution with automated control of all major wafer probing systems
SANTA ROSA, Calif., July 19, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today announced the newest release of its high-performance, Advanced Low-Frequency Noise Analyzer (A-LFNA), which is designed to make fast, accurate and repeatable low-frequency noise measurements. The release features a new user interface and tight integration with Keysight's WaferPro Express software — a platform that performs automated wafer-level measurements of semiconductor devices. As part of this larger framework, the platform provides engineers with a deeper understanding of the noise in their devices and circuits, surpassing dead-end noise measurements on a standalone system.
Today's semiconductor device characterization engineers often want a noise measurement system that is flexible and expandable. In particular, they require one that integrates advanced low-frequency device noise measurement and analysis with wafer-level measurements in a single, powerful platform that is capable of managing full wafer-level characterization. The seamless integration of Keysight's A-LFNA with WaferPro Express software offers just that functionality. This integrated solution facilitates noise measurements on components, individual devices and integrated circuits; both packaged and at the wafer level. Just as before, engineers using WaferPro Express can program and sequence high-speed DC, capacitance and RF S-parameters measurements, all the while automating wafer prober control. Now with the noise measurement module, they can add noise measurements and analysis to the test suite.
The A-LFNA's built-in measurement routines make DC and noise measurements turnkey. To measure noise on an N-Type MOSFET, for example, the system automatically chooses the source and load impedances that will best expose the intrinsic device noise. The engineer can accept these recommended settings or make changes, and a noise measurement is initiated. The A-LFNA then measures noise power spectral density (1/f noise) and noise in the time domain (RTN). Resulting data is plotted using a multiplot data display window. Various windows tabs help facilitate common tasks like evaluating device DC operating point and measuring the slope of the power spectral density curve. Noise data may also be analyzed and represented in device models using device modeling tools like Keysight's Model Builder Program (MBP) and IC-CAP. Circuit designers can use these device models to ensure highly accurate RF and analog low-noise circuit design.
"Our device characterization and modeling customers have diverse test needs, ranging from GaN reliability and CMOS modeling to magnetic sensors tests," said Todd Cutler, vice president and general manager of Keysight Design and Test Software. "With our new software user interface for the A-LFNA, we have given our customers the unique ability to measure and model device noise across their wafers, while still providing them full and flexible measurement options from DC to capacitance to S-parameters at microwave frequencies."
Keysight's A-LFNA features industry-leading noise sensitivity (-183 dBV2/Hz) that allows device modeling and circuit characterization engineers to quickly and accurately characterize devices at high voltages (to 200 V) and down to ultra-low frequencies (to 0.03 Hz). Such capabilities make it ideal for process design kit development by semiconductor foundries and for statistical process control during device manufacturing. IC manufacturers of operational amplifiers and linear voltage regulators can also use the A-LFNA to characterize the output voltage noise specification in their datasheets.
More information about the A-LFNA is available at www.keysight.com/find/eesof-a-lfna. Images of the analyzer are available at www.keysight.com/find/A-LFNA_images. A video on A-LFNA is available on YouTube at https://youtu.be/dE__pYPFX2U.
U.S. Pricing and Availability
Keysight's E4727A A-LFNA is available now. Contact Keysight at www.keysight.com/find/contactus for specific pricing information.
About Keysight EEsof EDA Software
Keysight EEsof EDA is the leading supplier of electronic design automation software for microwave, RF, high-frequency, high-speed digital, RF system, electronic system level, circuit, 3-D electromagnetic, physical design and device-modeling applications. More information is available at www.keysight.com/find/eesof.
About Keysight in Software
Keysight software is downloadable design, test and measurement expertise. From first simulation through first customer shipment, Keysight software tools enable engineering teams to accelerate from data to information to actionable insight. Additional information is available at www.keysight.com/find/software Download free software trials at www.keysight.com/find/free_trials.
About Keysight Technologies
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com