Highlights:
- New fast Fourier transform (FFT) application option now available on the 12-bit high-speed data acquisition PCIe® card
- Highly improved fixed point arithmetic that eliminates deteriorating effects
- Targeting applications in astronomy, physics and environmental measurements using FFT spectrometer
SANTA ROSA, Calif., April 20, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today introduced an improved version of the FFT option, now available on the U5303A PCIe 12-bit high-speed data acquisition card. This card features two channels and a sampling rate from 1 GS/s to 3.2 GS/s.
Designed for astronomy, physics applications and environmental measurements requiring frequency domain signal processing, the card allows observation of phenomena never observed before with previous instruments making it a big step forward in terms of linearity, dynamic range and spurious free dynamic range (SFDR) measurements. While providing continuous real-time FFT at full sampling rate, this option also enables spectra accumulation capability, a key requirement for radio-astronomy.
With DC up to 2 GHz bandwidth nominal, the card allows users to convert even low frequencies of around 0 Hz not observable with an AC front-end; moreover, AC coupling would introduce BF noise, whereas DC coupling provides measurement fidelity. By increasing the resolution from 8- to 12-bit, this option provides computation of a 32K points FFT for single or dual channels. As a result of its low-noise capabilities, the card allows users to detect phenomena difficult to observe, such as tilted fibers in solar burst. Additionally, in a controlled environment, this application can run at altitude of 15,000 feet.
Key features of the new FFT version include:
Key advanced functionalities include:
"Thanks to a remarkable dynamic range, this new fast Fourier transform version allows performance of sensitive observations in highly interfered environment," said C. Monstein, Radio Engineer at Institute for Astronomy, ETH Zürich. "With 12-bit resolution, the card enables observation of -110 dBm signals in -30 dBm interfered spectrum. Even in very strong FM band we can still see the solar radio burst structure without cross-modulation or ghosts, which wasn't possible before with previous instruments at ETH, such as Phoenix-generations, Argos, Callisto, and so forth. Keysight's on-going collaboration with the institute enables continuous technological improvements."
This application option comes with a dedicated FFT spectrometer graphic user interface, allowing fast initial start-up, display and export of the acquired FFT data.
Information about product configuration is available at www.keysight.com/find/U5303A. High-resolution images are available at www.keysight.com/find/FFT_PCIe_Digitizer_images.
Pricing and Availability
For pricing information about the applications option dedicated to fast Fourier transform, please contact digitizers@keysight.com.
About Keysight High-Speed Digitizers
Keysight's high-speed digitizers are the result of more than 300 years of cumulative research and development experience in analog-to-digital conversion technology. This ensures the ability to achieve the most effective and reliable analog-to-digital conversion at high-resolution and fast sampling rates. Information on the technology and its applications is available at www.keysight.com/find/high-speed-digitizers.
About Keysight in Modular
Keysight provides unrivaled PXI and AXIe performance built on the industry's most accurate measurement science. Keysight helps engineers get to first measurement faster with common measurement software and Keysight Reference Solutions. Keysight has the industry's largest global network of experienced application engineers and metrology-grade calibration centers. Additional information about Keysight's PXI and AXIe modular test and measurement solutions is available at www.keysight.com/find/modular.
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
PCIe® is a U.S. registered trademarks of PCI-SIG.
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com