SANTA ROSA, Calif., Oct. 17, 2017
Keysight Technologies, Inc. (NYSE: KEYS) today announced the successful demonstration of Gigabit LTE download speeds at the 2017 IAA Automotive Show (www.iaa.de). Featured as a part of Qualcomm Technologies Inc.'s infotainment demonstration, Keysight's E7515A UXM wireless test was used in combination with Qualcomm Technologies' connected car platform, which features the Qualcomm® Snapdragon™ X16 LTE modem, to achieve Gigabit download speeds. Together, the companies achieved sustained internet protocol (IP) data throughput of 1 Gbps speeds in the vehicle using three component carrier aggregation (3C-CA), 4x4 downlink MIMO and 256QAM modulation. The prototype vehicle also showcased an infotainment system powered by another flagship solution from Qualcomm Technologies—the Snapdragon 820A automotive processor.
The IAA 2017 International Motor Show is the world's largest motor show and was held in Frankfurt, Germany during the week of Sept. 14. This achievement is a testimony to the fact that Keysight is dedicated to working with the industry leaders in wireless and will remain at the forefront of technology.
"We are pleased to have worked with Qualcomm Technologies in this important event for the automotive industry," said Kailash Narayanan, vice president and general manager of Keysight's Wireless Device and Operators. "This demonstrates our continued commitment and effort towards deployment of next-generation wireless technologies through strong collaboration with industry leaders."
Additional Information
More information about Keysight's UXM wireless test set is available at www.keysight.com/find/UXM. High resolution images are available at www.keysight.com/find/UXM-images. Videos demonstrating the UXM's versatile capabilities are available on YouTube. Contact Keysight at www.keysight.com/find/contactus for E7515A UXM pricing and delivery information.
About Keysight in 5G
The development of 5G depends on up-to-date tools that let designers easily explore new signals, scenarios and topologies. Keysight's 5G solutions are ready to enable deeper insights as development evolves with the standard. In design and test, Keysight is helping industry leaders innovate across new and existing technologies as they transform ideas into reality. Additional information about Keysight's 5G design, test and measurement solutions is available at www.keysight.com/find/5G.
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps its engineering, enterprise and service provider customers optimize networks and bring electronic products to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2016. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
Qualcomm and Snapdragon are trademarks of Qualcomm Incorporated, registered in the United States and other countries. Qualcomm Snapdragon is a product of Qualcomm Technologies, Inc.
Contact:
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Magda Antone, Europe
+34 (93) 3434612
press.emea@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com