Highlights:
- New Type-C test controller (N7018A) sets the device to desired power state, orientation and alternate mode
- New versions of compliance software packages automate characterization and validation testing with the integrated N7018A test controller
- Sequencing software for receiver and transmitter test solutions provides testing of multiple standards without interruption or monitoring
SANTA ROSA, Calif., Sept. 18, 2017
Keysight Technologies, Inc. (NYSE: KEYS) today announced the N7018A Type-C test controller, which enables unfettered automated validation of USB 3.1, TBT 3, and DisplayPort over Type-C, and is a key component of Keysight’s high-speed validation systems. The N7018A can set contracts up to 100 watts and set devices into alternate modes (DisplayPort and Thunderbolt).
The N7018A enables complete test device control by routing SBU lines to industry-standard controllers for the alt mode testing and by providing low frequency periodic signaling (LFPS) signals for the control of USB3.1 devices. The test controller ensures faster bring up and debug by providing control and access of the Type-C interface’s CC, VBus and SBU lines. Engineers can operate the test controller from a stand-alone graphical user interface, or through an application programming interface (API) integrated into one of Keysight’s compliance applications.
New versions of Keysight’s compliance solutions, with the integrated N7018A test controller, are as follows:
|
|
|
|
|
|
|
|
|
|
|
“At Keysight, we recognize that it is critical to address the entire process of characterization and validation and not just the compliance regimen,” said Kailash Narayanan, vice president and general manager, Wireless Device and Operators. “The new Type-C Test Controller is a perfect example of this because it enables testing a Type-C device in any state, for all standards appropriate for that device, allowing the validation engineer to efficiently accomplish standard compliance test and corner case testing.”
Additional Information
More information about the N7018A Type-C test controller is available at www.keysight.com/find/N7018A. Images are available at www.keysight.com/find/N7018A-images.
Keysight Technologies is a leading technology company that helps its engineering, enterprise and service provider customers optimize networks and bring electronic products to market faster and at a lower cost. Keysight’s solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2016. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
Contact:
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com