Highlights:
- Delivers magnitude stability of less than 0.015 dB and phase stability of less than 0.15 degrees
- Enhances device characterization and modeling for connectorized and on-wafer measurements
- Extends time between calibrations with industry-leading stability
SANTA ROSA, Calif., May 22, 2017
Keysight Technologies, Inc. (NYSE: KEYS) today announced a broadband millimeter-wave network analyzer solution that delivers unparalleled system-level accuracy up to 120 GHz. The new Keysight N5290/91A solutions produce metrology-grade results that enable leading-edge developers to confidently characterize their millimeter-wave designs.
The new solution enhances device characterization and modeling by delivering exceptional stability and accuracy for on-wafer and connectorized measurements. Magnitude stability is less than 0.015 dB and phase accuracy is less than 0.15 degrees over a 24-hour period.
Leveraging Keysight's proven expertise in metrology, the solution's calibration capabilities are based on an improved-accuracy database that supports a 1.0 mm calibration kit (85059B) and a 1.0 mm verification kit (85059V). With this foundation, the new broadband millimeter-wave solution provides measurement results that are traceable to national metrology institutes.
Core elements of the system are a Keysight PNA or PNA-X network analyzer, along with N5293A Series compact frequency extenders and the N5292A test-set controller. To simplify benchtop measurements, engineers can mount the frequency extenders on an optional desktop positioner.
Ruggedized 1.0 mm test ports ensure repeatable connections that improve calibration uncertainty and therefore system-level measurement precision. Users can apply automatic fixture de-embedding to connectorized measurements or perform calibration at the probe tips during on-wafer measurements.
The optional 900 Hz start frequency, with Options 205 or 425, enables engineers to characterize the low-frequency performance of their devices. This is especially useful when measuring the low-loss transmission line structures that are commonly used in high-speed digital applications.
Keysight collaborated with solution partner Cascade Microtech to provide a complete wafer measurement solution (WMS) based on the N5290/91A and the Keysight W8580BP WaferPro Express Core Measurement Bundle (software, drivers and database). The WMS program provides guaranteed configuration, installation and support to reduce risk and accelerate time to first measurement.
The broadband millimeter-wave solution also supports a variety of Keysight's proven measurement applications. Examples include complete characterization of amplifiers and frequency converters (gain compression software option), measurements of mixers and frequency converters (scalar mixer software option), and calibrated multi-channel spectrum measurements (extended spectrum analyzer software option).
Enhancing Usability with a Streamlined Workflow
Keysight is also introducing a multi-touch user interface (UI) for all models in the PNA Series of network analyzers. Updates to the UI include a 12.1-inch widescreen display; easy access to frequently used functions; quick setups using touch-activated tabbed softkeys and dialog menus; and intuitive single- and multi-touch gestures to drag-and-drop or magnify traces.
U.S. Pricing and Availability
The following products are all available today at the indicated U.S. list prices:
Information about the N5290/91A broadband millimeter-wave network analyzer solution is available at www.keysight.com/find/millimeter-wave. Product images are available at www.keysight.com/find/broadbandmillimeterwavesolutions-images. A media backgrounder is available at www.keysight.com/find/broadbandmillimeterwavesolutions-backgrounder.
Keysight Technologies is a leading technology company that helps its engineering, enterprise and service provider customers optimize networks and bring electronic products to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2016. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on Facebook, Google+, LinkedIn, Twitter and YouTube
Contact:
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com