Highlights:
- Keysight now offers a transmitter and receiver test solution based on the MIPI® Alliance's D-PHYSM v2.0 and v2.1 specification and C-PHYSM v1.0 and v1.1 specification and conformance test suite (CTS)
- Keysight also supports MIPI Alliance's system power management interface (SPMI) specification protocol decoder for battery-operated Internet of Things (IoT) and mobile devices
SANTA ROSA, Calif., April 25, 2017
Keysight Technologies, Inc. (NYSE: KEYS) today announced a new MIPI D-PHY and C-PHY test solution to help accelerate the development of next-generation mobile and IoT devices. Keysight's new test solution supports the MIPI Alliance's D-PHY v2.0/v2.1 specification and C-PHY v1.0/v1.1 specification and conformance test suite. The test solution consists of the Keysight U7238E MIPI D-PHY compliance test software and the U7250A MIPI C-PHY compliance test software for Infiniium, as well as the Keysight DSAV164A digital oscilloscope for transmitter test and the Keysight M8085A MIPI Receiver Test Solution software package running on the M8195A or M8190A arbitrary waveform generator for receiver test.
The MIPI Alliance's new MIPI D-PHY and C-PHY specifications address several rapidly changing markets. For the virtual reality (VR) and augmented reality (AR) markets, each specification supports up to 9 Gbps and 11.4 Gbps (5Gsps) for the camera interface, enabling 8K 60Hz video recording. For the autonomous car market, which requires multiple camera modules and sensors for detecting environmental conditions instead of human's eyes, the new specification is important because it addresses the low latency and virtual channel support requirements without increasing cable harness weight.
Supporting these different markets requires higher data rate and more complex validation testing, which will become more challenging to the test and validation engineers versus previous specifications.
"Having adequate testing solutions for MIPI interface standards is an essential cornerstone for ecosystem enablement," said Joel Huloux, chairman of the MIPI Alliance board of directors. "Great to see that Keysight Technologies demonstrates their continuous support of MIPI standards with updated solutions that address current and future testing requirements."
For future testing needs, the Keysight solution can also provide an 8 Gbps D-PHY signal in one M8195A AWG module, and can synchronize two or more M8195A modules to generate a 16 Gbps D-PHY signal. For C-PHY, the test solution can generate up to 8 Gsps C-PHY signal.
IoT environmental devices depend on highly efficient batteries that last a long time and require less charging. The MIPI Alliance recently released a new interface to manage battery interface—the system power management interface (SPMI). Keysight's N8845A application decodes SPMI data from its Infiniium oscilloscope. This application helps reduce development time by providing proper triggering on specific packet and detailed decoding information.
"Keysight's MIPI test solution helps enable technical innovation in the mobile industry, providing a solution that ensures conformance to the evolving standards and data rates," said Kailash Narayanan, vice president and general manager of Keysight's Wireless Devices Segment. "Working with the MIPI Alliance and industry leaders allows us to offer a complete solution that covers the new MIPI D-PHY v2.0 and v2.1 specification and the C-PHY v1.1 specification and CTS test."
Keysight Technologies (NYSE: KEYS) helps customers bring breakthrough electronic products and systems to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in the network. Customers span the worldwide communications ecosystem, internet infrastructure, aerospace & defense, automotive, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2016. More information is available at www.keysight.com.
About MIPI Alliance
MIPI Alliance (MIPI) develops interface specifications for mobile and mobile-influenced industries. There is at least one MIPI specification in every smartphone manufactured today. Founded in 2003, the organization has nearly 300 member companies worldwide and 13 active working groups delivering specifications within the mobile ecosystem. Members of the organization include handset manufacturers, device OEMs, software providers, semiconductor companies, application processor developers, IP tool providers, test and test equipment companies, as well as camera, tablet and laptop manufacturers. Additional information is available at www.mipi.org.
# # #
MIPI®, D-PHYSM and C-PHYSM service marks and logo marks are owned by MIPI Alliance, Inc. and any use of such marks by Keysight Technologies is under license. Other service marks and trade names are those of their respective owners
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on Facebook, Google+, LinkedIn, Twitter and YouTube
Contact:
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com