Keysight Technologies Teams with European Space Agency, Airbus, SpaceTech GmbH to Evaluate Radar for Icy Moons Exploration Antenna

  
  

Tests of the instrument verify S-parameter performance of antenna as if mounted on spacecraft

Highlights:

  • Keysight FieldFox handheld RF analyzer used to test radar for icy moons exploration (RIME) instrument antenna for use in the Jupiter icy moons explorer (JUICE) spacecraft, European Space Agency's (ESA's) deep space mission to the moons of Jupiter
  • FieldFox measured characteristics of the antenna
  • The 16.6-meter antenna of the RIME instrument was tested in various flight configurations during a two-day campaign in September 2017

SANTA ROSA, Calif., Nov. 29, 2017

Keysight Technologies, Inc. (NYSE: KEYS) today announced that the FieldFox handheld RF analyzer was used in the evaluation of the impedance of the radar antenna for icy moons exploration (RIME), a key component of one of the ten science payloads of the European Space Agency's Jupiter icy moons explorer (JUICE) spacecraft scheduled for launch in 2022.

RIME engineers performed phase-matching and orientation tests on the RIME antenna in Heiligenberg, Germany in September 2017. They also evaluated two radar antennas, one aluminum and the other carbon fiber reinforced polymer (CFRP), which will be used on the spacecraft. The antennas were housed on a satellite-sized enclosure, and the enclosure was lifted 300 meters in the air by helicopter to ensure low-RF coupling to the ground.

Keysight's handheld FieldFox analyzer was used in remote mode to measure S-parameter characteristics of the antenna in flight as it was rotated more than 180 degrees and with the spacecraft mock-up being maneuvered by helicopter. Test data was recovered at a base station on the ground via a wireless link between the FieldFox and the ground base station.

"We are pleased at being chosen as a key test solution provider for evaluation of the RIME antenna," said Greg Peters, vice president and general manager, Aerospace, Defense, Government Solutions Group, Keysight Technologies. "By measuring the matching characteristics of a trial radar antenna, ESA and Airbus engineers can correlate design simulation with actual test data."

"The test was a fundamental step towards understanding the behavior of the real antenna that will ultimately allow us to perform highly accurate measurements of the radar echoes reflected from the deep subsurface of the Jovian icy moons," said principal investigator, Lorenzo Bruzzone, University of Trento, Italy.

Additional Information

The FieldFox family provides a choice of 22 combination (combo) and spectrum analyzer models with frequency coverage from DC to 50 GHz and users can configure combo models to include spectrum analyzer, VNA, CAT, RTSA and more. All models offer benchtop precision and are MIL-Class 2 rugged. More information is available at www.keysight.com/find/fieldfox. Images are available at www.keysight.com/find/fieldfox-images.

In addition to the risks above, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10-K for the fiscal year ended Oct. 31, 2016, and Keysight's quarterly report on Form 10-Q for the period ended July 31, 2017.


About Keysight Technologies

Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps its engineering, enterprise and service provider customers optimize networks and bring electronic products to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2016. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.

# # #

Contact:

Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com

Magda Antone, Europe
+34 (93) 3434612
press.emea@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com