SANTA ROSA, Calif., July 12, 2018
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises and service providers accelerate innovation to connect and secure the world, announced the new Infiniium UXR series, the only oscilloscopes to support terabit research with real-time bandwidth up to 110 GHz industry-leading sample rate (256 GSa/s) and signal integrity (lowest noise and jitter).
As the demand for faster and more data continues to surge, digital speeds increase and consequently, margins decrease. Test equipment has struggled to keep up with the cutting-edge researchers that are racing to the next technology breakthrough.
The Keysight Infiniium UXR series offers advanced capabilities that enable leading-edge researchers to accelerate time to market with PAM-4, 5G, and optical solutions, by ensuring signals are clearer, eye diagrams are open, and results are accurate. In addition, when paired with Keysight’s new up to 110GHz Optical Modulation Analyzer frontend and the VSA-based optical modulation software, the Keysight Infiniium UXR series turn into an end-to-end solution for optical research.
The Keysight Infiniium UXR series provides:
"The Infiniium UXR Series enables development teams to gain an extraordinary advantage in the race to beat their competition to market," said Ron Nersesian, Keysight president and CEO. "Only Keysight has the expertise to deliver a system that moves multiple performance points ahead simultaneously. The industry leading 110GHz bandwidth, low noise floor and jitter, enables the acceleration of new designs in high-speed digital, optical research, wideband wireless, and beyond."
Additional Information
More information about the Keysight Infiniium UXR Series real-time oscilloscopes is available at www.keysight.com/find/UXR. Images are available at www.keysight.com/find/UXR-images.
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on Facebook, Google+, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Magda Antone, Europe
+34 (93) 3434612
press.emea@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com