SANTA ROSA, Calif., May 07, 2019
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, announced a new dynamic power device analyzer with double-pulse tester (PD1500A) to deliver reliable, repeatable measurements of wide-bandgap (WBG) semiconductors, while ensuring the safety of the measurement hardware and the professionals performing the tests.
Global growth of the electric vehicle (EV) market is driving strong demand for small, high power, efficient electric power systems. As the industry turns to WBG semiconductor technology for mission critical applications like renewable energy and EVs, many power converter designers are hesitant to adopt this new technology due to potential reliability and repeatability risks in characterizing a new generation of semiconductors including insulated-gate bipolar transistor (IGBT), silicon carbide (SiC), and gallium nitride (GaN).
Fully characterizing a SiC or GaN device requires static and dynamic measurements. Keysight's B1505A and B1506A Power Device Analyzers deliver these static measurements and, with the addition of the new PD1500A, now also provides the flexibility needed to address a variety of dynamic measurements. This functionality is key since the standards for WBG devices, established by the Joint Electron Device Engineering Council (JEDEC), continue to evolve. JEDEC is a semiconductor trade and engineering standardization organization.
Keysight's PD1500A is designed to be modular, allowing many device types to be tested and different characterization tests to be performed at a variety of power levels. The initial system provides complete double-pulse test characterization and parameter extraction for Si and SiC power semiconductors with ratings up to 1.2 kV and 200 A. Additional modules will be added to the PD1500A in the future to perform tests on devices requiring more current, such as GaN and power modules.
Keysight's new PD1500A Dynamic Power Device Analyzer with Double-Pulse Test Capability provides reliable, repeatable measurements of wide-bandgap (WBG) semiconductors that enable customers to:
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.9B in fiscal year 2018. More information is available at www.keysight.com.
# # #
Related Images | ||
Keysight’s new dynamic power device analyzer with double-pulse tester - PD1500A |
Keysight’s new dynamic power device analyzer with double-pulse tester - PD1500A |
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news, and on Facebook, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662 4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660-2162
fusako_dohi@keysight.com