SANTA ROSA, Calif., January 8, 2019
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, today announced the 200 MHz, 4-channel models of the InfiniiVision 1000 X-Series oscilloscopes, providing professional-level measurements and capabilities at an affordable price, including 4-wire Serial Peripheral Interface (SPI) decode and remote connection via local area networks (LANs).
The new InfiniiVision 1000 X-Series oscilloscopes use the same user interface and measurement technology found in the higher performance Keysight InfiniiVision oscilloscopes. The intuitive front panel is easy-to-use and features built-in help enabling customers to quickly understand oscilloscope functions and improve overall test efficiency. Seventeen complementary training signals are preloaded to ensure rapid use of the advanced measurement and analysis capabilities inherent in the InfiniiVision 1000 X-Series. These training signals can also be used in conjunction with the free educator's training kit, which includes a comprehensive oscilloscope lab guide and oscilloscope fundamentals slide set.
"Visualizing electrical signals to understand both timing and voltage relationships is one of the most important sources of insights for the electrical engineering community," said Teit Poulsen, director, Altoo Measurement Science. "Keysight's new 4 channel DSOX1000 series oscilloscopes provide the highest level of signal insight and functionality at an unprecedented low price point while retaining the legendary Keysight quality. Allowing more engineers greater insight in the behavior of their electrical designs."
The new InfiniiVision 1000 X-Series models are bandwidth upgradable via software license, enabling customers to purchase the bandwidth needed now, and upgrade as designs evolve in the future. The InfiniiVision 1000 X-Series oscilloscopes are available at 70, 100, and 200 MHz of bandwidth and accelerate innovations with:
"We had quality in mind when developing the new 4-channel 1000 X-Series models. The industry needs measurements they can count on to make correct design decisions, at a price they can afford," said Dave Cipriani, vice president and general manager of Keysight's Digital Photonics Center of Excellence. "By leveraging proven technology used in our higher-end oscilloscopes, Keysight is offering customers measurements they can trust."
Additional Information
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.9B in fiscal year 2018. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news, Keysight blog, and on Facebook, Google+, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662 4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660-2162
fusako_dohi@keysight.com